BGT24LTR11 VCC_DIV and DIV

Announcements

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
h_nakamura
Level 5
Level 5
Distributor - NEXTY (Japan)
10 solutions authored 50 questions asked First like received

Hi,

If you don't need the frequency divider, it's open (nothing is connected)
Is there a problem using it?

 

h_nakamura_1-1657519091044.pngh_nakamura_2-1657519105863.png

 

Best regards,

nakamura

0 Likes
1 Solution
Honey_D
Moderator
Moderator
Moderator
5 comments on blog 50 likes received 250 replies posted

Hi @h_nakamura ,

The connections are advised when ones want to monitor the frequency divider output. In order to monitor the DIV_OUT (frequency divider output from BGT24LTR11) assemble R38 (0 ohm) and VTUNE (VCO frequency tuning voltage) assemble R39 (0 ohm) 

HoneyDhandhukia_0-1657601218229.png

Hope this helps

Best Regards

Honey

View solution in original post

5 Replies
Honey_D
Moderator
Moderator
Moderator
5 comments on blog 50 likes received 250 replies posted

Hello @h_nakamura ,

The output of the frequency divider are open so as to provide the flexibility to use it with different configuration to control the VCO using a PTAT, PLL or a software based open-loop concept. Please refer to the section 4 VCO Control from the user guide for more details .

Hope this helps

Best Regards

Honey

0 Likes
h_nakamura
Level 5
Level 5
Distributor - NEXTY (Japan)
10 solutions authored 50 questions asked First like received

Hi Honey,

Thnanks for your prompt reply.
Is it mean that the VCC_DIV and the DIV pins don't need to be pulled up or pulled down when these pins aren't used?

B.r
nakamura

0 Likes
Honey_D
Moderator
Moderator
Moderator
5 comments on blog 50 likes received 250 replies posted

HI @h_nakamura ,

Yes, the pins can be used as per the requirement, as it is been used in Sens2GoL Pulse as explained in the application note

Hope this helps

Best Regards,

Honey

0 Likes
h_nakamura
Level 5
Level 5
Distributor - NEXTY (Japan)
10 solutions authored 50 questions asked First like received

Hi,
The AN597 does not have a direct description when it does not use pins, but from the description in "4.5.5 Prescalar" it can be inferred that it is "open" when it is not used because it requires a connector connection when used. Is this understanding correct?
R38 (0Ω) is for VCC_DIV.
R39 (0Ω) is for DIV.

Best regards,
H.N

0 Likes
Honey_D
Moderator
Moderator
Moderator
5 comments on blog 50 likes received 250 replies posted

Hi @h_nakamura ,

The connections are advised when ones want to monitor the frequency divider output. In order to monitor the DIV_OUT (frequency divider output from BGT24LTR11) assemble R38 (0 ohm) and VTUNE (VCO frequency tuning voltage) assemble R39 (0 ohm) 

HoneyDhandhukia_0-1657601218229.png

Hope this helps

Best Regards

Honey