Public Archive Forum Discussions
hi expert,
I've downloaded the FX3 development kit, and I saw the CYUSB3014 EZ USB FX3 datasheet.pdf in documents folder,
But there is no detailed SOC information, such as the registers, and arm core information.
I think this should be in the TRM.
Where can I get such kind of information? or where to get the TRM?
Thanks.
Show LessNote: SDK 2.1.0 requires the WICED SMART BCM92073X_LE_KIT small form factor development board and cannot be used with older BCM920732_LE_KIT development boards.
WICED™ SMART Software Development Kit (version 2.1.0)
The WICED Smart SDK includes the tools and software needed to create BLE peripheral and central devices for a wide range of products.
The SDK is available as a standalone compressed file or as a separate installer bundled with the WICED™ Integrated Development Environment.
This .7z version of the WICED™ SMART SDK can be used to integrate with an existing Eclipse installation on Windows, Linux or MAC OS.
Show LessVideo Introduction to WICED Smart (7 minutes).
Video Introduction to WICED Wi-Fi (7 minutes)
Attached is some code I received from the development team that demonstrates deep sleep enablement and the associated clock source handling within SDK 2.x
Show LessWhen I try to build any project with Cypress EZ USB Suite, I always get the error:
cs-make: *** Access is denied.
I am using the latest version of the tools on a Windows 7 64-bit machine.
Does anyone have any suggestions?
Show LessPreliminary iOS Source Code Guide
More later...
Hello,
I'm a beginner in the FX3 tools and could not study all the UGs and HBs yet.
I cannot understand the GNU Tollchain and the Eclipse USB Suite using.
Both tools can be used to develop projects based on C++. Am I right?
But the first brings you to the command line and the second one to the windows interface. Am I right?
What tool is preferable for a beginner?
Are there any restrictions in these tools using?
Thank you,
tduty
Show Less