cancel
Showing results for 
Search instead for 
Did you mean: 

Public Archive

Anonymous
Not applicable
2 Replies
Anonymous
Not applicable

P39 is listed in this document as being the CS line for SPI2 slave while


IN short I cannot use the documentation to construct a board. I don't trust it.

If there was a schematic of a BCM20736S application, lets say your version of the CC2541 SensorTag Board it would be a great help.

0 Likes
MichaelF_56
Moderator
Moderator

Note that the Hardware Interfaces is written from the perspective of the SOC, which supports more functionality than what is brought out on the module.

The schematic for the TAG board is here: BCM92073X_LE_KIT Schematics, Layout, Firmware

There are some good external oscillator threads here: WICED Smart Forums

0 Likes