WICED Sense Reference Design Bill of Materials
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
WICED_SENSE_BOM - Bill of Materials (WICED_SENSE_V1.0_BOM_V0.2.xlsx).

0 Likes
2 Replies
Anonymous
Not applicable

Hi J.T, MMFAE,

I don't see the series opposing Zeners viz. D3, D4,D5 etc... in the BOM document.  Are they DNI'ed.

Thanks.

0 Likes
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

These opposing zener diodes offer some protection against anything above 10V. In fact we have D4,D5,D6,D9 and D10. The schematics did not identify any part number nor can I make out if they were installed from the layout. I guessed they are not installed.