I've solved the problems with the libraries, but now i've got another one:
It's written in the readme, that the application binary will be copied to /usr/bin and can be launched using 'cyusb_linux' comand. Using this comand in the terminal gives:
cyusb_linux: error while loading shared libraries: libcyusb.so: cannot open shared object file: No such file or directory
But i've located this file in /usr/lib
Is that ok?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am facing same problem. Can anyone help on this.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
( As a prerequisite, ensure that you have qt4, gcc and libusb installed in your linux machine)
After downloading the SDK ( use the latest SDK 1.3.1 available here), Go to <your path>/fx3_sdk_v1.3.1_linux/ cyusb_linux_1.0.4/ directory
run the make command in the terminal followed by ./install.sh (Steps given in the README file in the same directory)
Running install.sh script with root privileges should copy the libcyusb.so and libcyusb.so.1 into /usr/local/lib directory
Now, you can launch GUI applications using cyusb_linux command. Make sure to run the application as normal user.
However, if you get this error cyusb_linux: error while loading shared libraries: libcyusb.so: cannot open shared object file: No such file or directory, You will have to manually export the library by typing the following command
export LD_LIBRARY_PATH= /usr/local/lib/
Also, Add this above line to end of .bashrc file in home folder so that you dont have to do this for every session. ( .bashrc is a hidden file in home directory and can be made visible by pressing Ctrl+h)
After exporting the library, you can now launch GUI applications using cyusb_linux command
Regards
Mudabir Kabir
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mudabir,
Quote
Running install.sh script with root privileges should copy the libcyusb.so and libcyusb.so.1 into /usr/local/lib directory
Now, you can launch GUI applications using cyusb_linux command. Make sure to run the application as normal user.
I'm working in a rasberry pi device.
I ran the install.sh script as root and everything looked good. Then...
When I run as normal user (pi) ./cyusb_linux and there is cypress hardware connected I get this:
Error in opening device
Error opening library
If there is no usb cypress hardware connected It opens and give me a message in command line:
No device found.
If I plug the usb cypress hardware, cyusb_linux program closes and gives this messages in command line:
Signal 10 (=SIGUSR1) received !
Error in opening device
Error in opening library
When I run sudo ./cyusb_linux it runs good and normal.
Any advice?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I got this response and works like a charm!
Hi Gabriel,
Open /etc/udev/rules.d/88-cyusb.rules as sudo and change the included rules to:
KERNEL=="*", SUBSYSTEM=="usb", ENV{DEVTYPE}=="usb_device", ACTION=="add", ATTR{idVendor}=="04b4", GROUP="user_group", MODE="666", TAG="cyusb_dev", RUN+="/usr/local/bin/cy_renumerate.sh A"
KERNEL=="*", SUBSYSTEM=="usb", ENV{DEVTYPE}=="usb_device", ACTION=="remove", TAG=="cyusb_dev", RUN+="/usr/local/bin/cy_renumerate.sh R"
where user_group is a group that the user is a member of.
If you want only one specific user to access the device, you can change it to:
KERNEL=="*", SUBSYSTEM=="usb", ENV{DEVTYPE}=="usb_device", ACTION=="add", ATTR{idVendor}=="04b4", OWNER="username", MODE="666", TAG="cyusb_dev", RUN+="/usr/local/bin/cy_renumerate.sh A"
KERNEL=="*", SUBSYSTEM=="usb", ENV{DEVTYPE}=="usb_device", ACTION=="remove", TAG=="cyusb_dev", RUN+="/usr/local/bin/cy_renumerate.sh R"
For the second part of question
"Undefined reference to 'cyusb_open()'"
You need to link to cy_lib.
You can add the following line in your make file.
g++ -o 00_fwload 00_fwload.c -L ../lib -l cyusb
If you have any queries please get back to us.
Thanks & Regards,
krishna GSNS.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm working in raspberry pi device. the cyusb_linux application is running with the above mentioned modifications. However, the examples 01_getdesc and other examples doesn't seem to run! from the terminal.
When I run as normal user (pi) ./01_getdesc and there is cypress hardware connected I get this:
Error in opening device
Error opening library
If there is no usb cypress hardware connected It opens and give me a message in command line:
No device found.
But with root privileges the application is working perfectly fine.
Can somebody give me advice on this regard?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
In install.sh, the command qmake-qt4 results in a failure.
I believe qt commands has changed since this guide was written, how do you get around thaT?
I have qt creator 5 installed on the pi, but still qmake-qt5 is command not found