Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Have completed page read/write operations for S34ML01G2. But for a particular page the data read is not equal to the data written and also the write status for that operation doesn't show any failed status. What can be the problem. How to solve??

Anonymous
Not applicable

Have completed page read/write operations for S34ML01G2. But for a particular page the data read is not equal to the data written and also the write status for that operation doesn't show any failed status. What can be the problem. How to solve??

0 Likes
1 Solution
Scott_Heo
Employee
Employee
First like given 5 solutions authored First solution authored

Hi Vinay,

Writing page data area (2048 bytes) looked like that the NAND driver didn't consider writing calculated ECC data to the NAND spare area accordingly. Basically, S34ML01G2 NAND requires max 4 bits error correction per in every 512 bytes of page area, and the correction should be done by a NAND driver - programming operation will not return a failure status but could have 4 bit errors in every 512 bytes. That means, before programming, the NAND driver needs to calculated ECC data per 512 bytes and the should be programmed to spare area accordingly. When you read the page data for a programming verification, you need to read page data and ECC data together, and then check the page data integrity using the ECC data read. If an error number exceeds 4 (per 512 bytes), then the driver need to manage the block as a bad block generated.

Thank you.

View solution in original post

0 Likes
4 Replies
Anonymous
Not applicable

Hello Vinay,

Can you please let us know how many bytes you are writing and how man you are reading back. ?

Did you try writing different no of bytes and observe the same issue ?

Is it happening on multiple pages or only in one page.

Is it possible for you to send the images of the data which you are writing and the data you are reading ?

Thanks,

Krishna.

0 Likes
Anonymous
Not applicable

Hi,

I am writing complete page data area (2048 bytes) with values 0x00 for all bytes. When I read the page data back I can see 1756th byte value as 0x02 and all remaining are 0x00. I thought the program page operation was success because read status register giving value 0xE0 after page program.

I found same issue for several blocks with different pages and offsets, but the page program operation was success.

0 Likes

Hi,

Based on your description, it seems like the Bad Block happened on your flash. Bad Block is normal on NAND flash due to the physical character.

Please refer the following KBAs about how to recognize and mark the Bad Block and our Bad Block limit:

Bad Blocks in NAND Flash Devices - KBA215722

Marking and Recognizing Bad Blocks in NAND Flash - KBA219305

Thank you!

0 Likes
Scott_Heo
Employee
Employee
First like given 5 solutions authored First solution authored

Hi Vinay,

Writing page data area (2048 bytes) looked like that the NAND driver didn't consider writing calculated ECC data to the NAND spare area accordingly. Basically, S34ML01G2 NAND requires max 4 bits error correction per in every 512 bytes of page area, and the correction should be done by a NAND driver - programming operation will not return a failure status but could have 4 bit errors in every 512 bytes. That means, before programming, the NAND driver needs to calculated ECC data per 512 bytes and the should be programmed to spare area accordingly. When you read the page data for a programming verification, you need to read page data and ECC data together, and then check the page data integrity using the ECC data read. If an error number exceeds 4 (per 512 bytes), then the driver need to manage the block as a bad block generated.

Thank you.

0 Likes