CyBluetool (Windows Installer)

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

CyBluetool is a GUI tool for testing and debugging Cypress Bluetooth devices. CyBluetool connects to the Bluetooth devices at HCI protocol layer and currently supports HCI UART and HCI USB transport interfaces. The tool allows user to send Bluetooth(BT) HCI commands and receive BT HCI events from the BT controller of the connected devices.

The .zip file contains a self extracting executable which includes both the program installation and the latest CyBluetool User Guide.

2 Replies
lock attach
Attachments are accessible only for community members.
szchen2006
Level 1
Level 1
10 sign-ins 5 replies posted 5 sign-ins

Hi, Sir/Ms,

I have one question for you:

when I was trying to download the application code into the extra SPI Flash of CYW920706WCDEVAL, it reprots some errors to me. Can you help with this?

Thanks,

0 Likes
wanglei3758
Level 1
Level 1
First reply posted First like given Welcome!

Whether there is WIFI debugging software?

0 Likes