Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Recent discussions
Hello,
I need to buy a compiler for the FX2LP18 USB microcontroller CY7C68053. Can you confirm that the Keil PK51 is compatible with the CY7C68053?
Thank you
Best Regards,
Patrice
Show LessInfineon's EZ-USB FX3S and SD3 support both support RAID 0 and RAID 1. Do any products support other RAID levels, specifically RAID 5?
RAID 0 is Block-level striping without parity or mirroring
RAID 1 is Mirroring without parity or striping
RAID 5 is Block-level striping with distributed parity
Greg
Show LessHello,
I am trying to generate an output frequency of 6 MHz using a PSOC 6 prototyping board but every time I measure the pin using an oscilloscope its not giving me the required frequency. I have attached the project. Can anyone help please?
Thank you
Show Less
hi,
i use the tasking to develop the TC1767,and i want generate a bin file ,
so i input cmd the post_build steps ,cmd follow
srec_cat.exe "F:\ITEC\infineon\taskingworkspace\LED_Blinking\Debug\LED_Blinking.hex" -intel -offset 0xA0000000 -o "F:\ITEC\infineon\taskingworkspace\LED_Blinking\Debug\1.bin" -Binary
but it have some wrong
it generate a large bin file. what should i change the rule ?
Regards,
sea
Show LessHi,
I bought the DEMO BGT60TR13C board and was able to run Radar Fusion GUI with the board successfully and was able to build an SDK from the source and run Presence Sensing App by following the steps for building Visual Studio Solution File (*.snl) using CMAKE on windows 10, 64-bit machine. The visual studio version I am running is the 2017 version.
So far in my understanding, the presence detection.exe built by the visual studio after building the presence sensing app is running the default configuration values for presence detection, as mentioned in the PRESENCE_SENSING_DEFAULTS_H.
Now my confusion starts here, how do I change the default values and apply them to the firmware that is being flashed to the DEMO BGT60TR13C board? after reading RDK it states by changing the values in the file config_presence_detection.json in the ...\RDK-TOOLS-SW\SDK\apps\c\share folder and then using bgt60-configurator-cli.exe to convert the config_presence_detection.json file into register list which needs to be copied and pasted to presence_sensing_defaults.h file?
Am I correct in my understanding? or am I missing something? please help me by explaining step-by-step procedures on how to change the reflect the changed parameters in the config_presence_detection.json file into firmware that is being flashed on the DEMO BGT60TR13C board. Also, how do I verify during the run-time of the Presence Sensing App on the DEMO board what are the segmentation parameters for presence sensing?
Thank You
Show Less
I can't find “Disassembly Window” here.
From the Debug menu, choose Windows > Disassembly.
Hello ALL,
in the software, there is a setting page about the basic working params of the system, shows below,
question, what is the meaning of Switching Frequency?
carrier signal frequency or IGBT gate switching frequency?
Thank you
Show Less
Hi, Infineon
I have tried to test the tle9879 deme kit.
But seems can not find the device use my Jlink version of V7.52c.
Could you please help check how to fix it?
Show Less
Hello,
I am trying to generate a frequency of 6 MHz using a Psoc 6 prototyping bord. Can you please check the attached project if this is correct?
Thank you
Show Less