Product Forum Discussions
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Recent discussions
Hi!
We are have an embedded system that is running vxworks 7 with the SLB9670VQ20FW785 TPM.
And we are currently investigating how to implement a software for provisioning our systems during manufacturing according to IEEE 802.1ar.
So I would like to know if it's feasible to store the Attestation Key certificate and the IDevID certificate on the TPM nvram?
I have no prior experience working with PKI/TPM/certificates and would greatly appreciate all the help I can get.
Show Less
Hello,
I am working with the 202007 BLE module and I have an external antenna connected to the uconnector and am receiving signal strength of -80dBm to -90dBm. I have done nothing to modify this device. Had anyone else had this issue?
Thanks
Show LessHi,
I'm using psoc6 with bless and mtb2.4.
I want my devices in peripheral mode to accept connection from public device adress and Random device adress.
I'm now able to do this in my code if i know before wich device will try to connect ( public or RPA)
In case of public address I set Cy_BLE_SetAddressResolutionEnable to false and it works.
In case of RPA i set Cy_BLE_SetAddressResolutionEnable to true and it works.
My question is the following : I need to allow connection from all kind of devices (public and RPA). Do I need to set Cy_BLE_SetAddressResolutionEnable to true? How can i add Public device address to Resolving List ? (that's what I do but it's not working...)
Thank you for your support,
Regards
Show LessHello,
I'm trying to flash a TLE987x EvalBoard with a TLE9872QX with a new µIO-Stick but it is not possible to connect it to the target. I connected the µIO-stick to the eval board powered with 12V external supply .
I
I'm using BSL_Tool application from the BSL-TOOLS_2022-02-26 package with Windows 10.
When I launch BSL-Tools, the "Connect" button is orange, it means the µIO-stick is recognized by windows
In the peripheral manager in windows, no error is detected.
I didn't update the µIO-Stick, because previously, I updated an other µIO-Stick with the firmware available in the BSL-TOOLS_2022-02-26 package (bsl_1.1.867) but it seems it bricked (now Windows can't recognize it). Then I bought a new µIO-Stick. It seems the current firmware of my new µIO-Stick is 3.0 (verified with Config Wizzard).
Then when I push on the "Connect" button, nothing happen. The status stay disconnected and I can't update my target.
I don't know if it is normal, but the red led (ERR) in the µIO-Stick is turned on and the orange led (ACT) is blinking.
Someone has an idea where does come from my problem?
Thanks.
Show Less
Hello,
I have updated my new uIO stick according to the manual by executing "UpdateBSL.cmd".
Now the stick is not recognised as HDI device any more.
Unfortunately I did not make a screenshot of the console after the update, the only thing I remember was, that after programming it said to press "any key" to continue and then the console closed.
On the device it self there is only the 5V and 3.3V LED green – no other LEDS are on.
I guess fw update might faild and the device is no dead. Is there a change to program the uIO stick with j-link or Lauterbach?
BR
Show Less
Hello,
I'm looking for a replacement of component marked as IOR P544H G6B8 F7017 (no sure 7017 or 7x17) - like on the picture.
Could you help me to identify this part and find replacement for that?
Thank you in advance for your help.
Unfortunately I can't find the size of the D-Flash1 on the TC322 chips. The product data sheet only lists the D-Flash0, which is marked as being 96kB. But what about the D-Flash1 for the HSM, is it 128 kB like for the bigger Aurix products or has it been gutted similarly to 96kB?
Show LessHello,
as the SGB02N120 IGBT is discontinued I am looking for an alterantiv part.
Looking at the listed IGBTs with 1,2kV there is no part with the same package or current.
Which transistor could be proposed?
Kind regards
Datasheet SGB02N120 (infineon.com)
Show LessHi, i'm testing the IFX007 motor control shield with a little (2.5W) brushed motor at 12V. The full-bridge .ino example works as expected but I cannot measure a proportional (is) current sense on the arduino board. I've also measured the voltage at the (is_rc) pin from duty cycle 0 to max (255) and the result is always 40mV.
What's is the problem to read the is current? How can I sense the high/low side mosfet currents?
thanks in advance,
gaston