All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
Dear forum:
I write hex file to flash by cypress programmer.
I can write the hex file normally, but when I open the cypress programmer,
but why the Chip protection is UNKNOWN?
Thank you.
Comment: My soft don't touch the eFuse address.
Show Less
Hello
Can we allocate 2 nodes on MULTICAN_CONFIG_0, and operate all message objects of both the nodes using only one CAN_Rx and CAN_Tx through transceiver??
Hello together,
I'm new here and stepped into an issue: We want to use the oscillatior monitor for a TC364 and the example in the user manual is to set the lower and upper threshold to +/-10% of fPLL0.
As the back-up clock is used as reference I assume this will fail because the datasheet grants only an accuracy/tolerance of +/-30% of the back-up clock.
So my question: is it necessary to trim the back-up clock, and how is this done?
In my understanding the finetrimming is not possible while runtime, without a trustable reference clock. So this should be an end of line process of the fnished product.
But there is a bit which controls the temperature based dynamic trimming. Does this help to switch on? And if this is recommended, why is it possible to switch on and off - then it should be always on. IMHO it makes only sense to deactivate this if the functionality is broken.
Can someone help with this issue?
best regards,
Thomas
Show LessHi support,
I would like to set-up a UART connection on my NAC1080 using the GPIO0 and GPIO2 in order to communicate with my PC the messages that the NAC1080 will be sending.
I've been reviewing the uart_drv.h library you have available and what I can't see is how the data transmission works.
There's a function called "transmit_bytes()" that send the Tx buffer data, but where's the Tx buffer?
How could I edit the data on that buffer to be able to send the desired message?
Regards,
-K
Show Less
Dear Sir,
I need an AUX power under 10W ,3.3V application which Input DC Vin 150V.
I saw the Coolset product - EVAL-ICE2QR1765Z. (provide a voltage of 70VDC to 380 VDC depending on the mains input voltage.)
Input voltage 85Vac~265Vac
Input frequency 50Hz, 60Hz
Output voltage and current 5V 2A
Output power 10W
can I follow the EV kit of EVAL-ICE2QR1765Z and take off bridge rectifier BR1 to work with input VDC at 150V?
thanks.
Show Less
I'm using IMI111T IC. I'm trying to connect to Imotion Solution Designer, but it's not connecting.
1. Install as an all user item during the program installation process.
2. Microsoft Visual was already installed, so I moved on.
3. Program writing is successful through the Programmer Tab through the I Motion Link.
4. Restart connecting when you go to the Dashboard -> Failed to connect with the target
I've replaced the IC about 2 times, and I tried with 3 laptops, but the same result came out.
Please advise connect.
#IMI111T
#i motion
Show LessNow we can modify the source pdo use dpm_update_src_cap() , CCG5 send source capability to device, and we want to know if there is any function can get the rdo from device
Show LessHello,
I am trying to use MULTICAN with XMC4700 Relax Kit, But i am unable to transmit data over it. I have attached my project below -
Please check my code and help me out with solution.
What is the magnetic hysteresis of the TLI5590 sensor? Does it differ on the two bridges?
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023