All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
From a linux system, I want to read back the configured program image from a CYC65215 part and check that its CRC is correct -- assuming it has an appended CRC. Does the image have a CRC? Is the CRC generated using a known algorithm with a standard polynomial? If so, which polynomial?
Show Lessin TC38x,Can the local memory unit(LMU) and thre Distributed LMU (DLMU) as a whole LMU to be used in OVC function SAL-TC387QP-160F300S AD
Show Less你好
目前使用"UART_VCOM_1_KIT_TC397_TFT"範例在Triboard TC397上進行測試。
開啟兩組ASCLIN 模組0跟模組4並且在中斷設置中有更改相對應的向量表數值,進行以下交互測試:
1. CPU0_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(0)"跟進行輸出"Hello World!" ==> 可以正常顯示
2. CPU1_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(1)"跟進行輸出"Hello World!" ==> 無法顯示
3. CPU2_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(2)"跟進行輸出"Hello World!" ==> 可以正常顯示
4. CPU3_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(3)"跟進行輸出"Hello World!" ==> 可以正常顯示
想請問為何在CPU1_Main.c會有此問題?
#AURIX
#Tricore
Show Less
when try to debug the example project through miniwiggler, it can not work as below:
but memtool can connect the chip :
MCD basic client can also connect the chip and get the information:
the ADS version is 1.9.20 ,DAS version is 8.0, miniwiggler is V3.1, hardware board is designed by other people and can be connected through UDE/pls
Show Less
Dear Forum:
I know that
The Hex file generated by the Modus Tool box IDE follows the Intel Hex File format which is supported by the Cypress Programmer.
from the following title.
https://community.infineon.com/t5/PSoC-6/PSoC-programmer-parsing-failure/td-p/716946
I want to confirm that
Which IDE can generate hex file used by PSoC programmer?
Thank you.
Show LessHi, the XDPS2201 is an asymmetric half-bridge flyback controller, but the XDPS2201 technical manual is AC-DC applied to USB PD .
1、May I ask if the chip XDPS2201 can be used in DC-DC applications?
2、If possible, how do the peripheral parameters of the chip (e.g. HV pins) need to be optimized to be suitable for DC-DC applications?
3, What is the best DC eyewire voltage range for the available pairs? Is it 48V DC, or does it have to be a high voltage bus 100VDC or 270VDC?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%B1%A0%E7%AE%A1%E7%90%86IC/XDPS2201%E5%8F%AF%E4%BB%A5%E7%94%A8%E4%BA%8EDC-DC%E5%BA%94%E7%94%A8%E5%90%97/td-p/723274
Show Less
Help!
Customer said my label is not original. Please help to verify. Thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/IRFR9024NTRPBF-label-question/td-p/723829
Show LessDear team need to understand why the upper limit for overtemperature is locked?
Also please confirm if there is any sample code for handling overtemperature
Show Less
Dear Team,
I am using the sequencer for analog input reading, just want to know what is difference between interrupt method and sequencer method for ADC1 reading?
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023