All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
What is the maximum output current limit for Vout 1 and Vout2 pin of S6AE102A / S6AE103A PMICs? I could not get this information in datasheet.
Show LessInstalled PSoC creator 4.2 to program the CY8CKIT-050 with the 5LP. I can no longer see the options to create a project for this hardware. What should I choose? The kit selection option is greyed out, and the alternatives are unclear if will work correctly.
Thanks
Show LessHello,
is it possible to use 2 SAR ADCs interleave to get 2 MSPS by supplying an external clock accordingly and assemble the signal after that again?
Anyone ever tried this?
Show LessI am practicing setting up DMAs by using the examples given here:
I would like to be able to change the phase of the sine wave by using a potentiometer. Does anyone have any tips on how to accomplish this?
Show LessHi,
can a PSoC5LP be a LIN master? There is a LIN component, but this seems to be a slave only.
The LIN protocol seems to be relatively slow, e.g. 19200bps. Does anyone have experience with LIN and is willing to share?
Best regards,
Turtle
Addition:
In the mean time I found out that there is a component named LIN USART in some PSoC1 that can be used as a LIN master.
As far as I understood is the problem the main problem the synchronisation gap at the beginning that is longer than a byte sent by the UART so that the UART can not generate this signal. Shouldn´t it be possible to use a AND to combine a control register bit and the UART output to generate this sync gap?
I have to send only one constant packet to make one sensor reply.
Show LessI've been running in circles trying to get an arrangement working which would allow me to send debugging information from a target board using a PSoC4 BLE chip to a laptop computer when using MINIPROG3. There are a number of comments and articles that talk about this but I've been unsuccessful at making any of them work. Further, when it seemed like I might have a solution it came at the expense of disabling the use of the regular debugging and programming functions.
Finally, I decided to set up a completely separate path from that of the MINIPROG3. The attached file is a very simple description of how this can be done along with a program that actually works in this regard. It uses an inexpensive FTDI Serial to UART converter cable available from Amazon.com. The connections and how to make it work are described at the top of the program. I have taken this approach to showing how I did it since I've often been frustrated with answers to questions that assume knowledge that I don't yet have. Perhaps this will be of help to someone else. I plan to add a two pin connector to every board I design to allow connection of the FTDI cable for future use. (At least until Cypress adds the capability to the MINIPROG3).
Dennis Coburn
Show LessWhen I create a project in creator 4.2 the USB UART does not work. When I use the RTC example project it does. I traced it to missing stdio.h in the new project. Is my install of creator bad and how do I fix it?
Show Lesshi,everybody
when i use the miniprog3‘s dll to develop my programmer,some question hit me。when i invoke the API <DAP_Acquire(string OUT strError)> of the miniprog3 to program my “.hex” into MCU,but if miniprog3 cannot acquire the mcu,it’s will cost 120-second to acquire the mcu and timeout,its so long for quantity production。
so how can i drop the timeout for the miniprog3 acquiring the chip ?
Thanks!
Show LessI have put my micro into sleep mode by disabling all the interrupts and using these (_WFI and _disable_irq ) instructions . I am not sure how to wake up my Micro from sleep mode by using interrupt.
Kindly give me some help and suggestions.
Thanks . Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023