All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
text.format{('custom.tabs.no.results')}
Hi,
I am looking to attach cheap NAND flash via SMIF to PSOC6.
I was able to place a 1Gbit part from Winbond onto the PSOC evaluation kit and have it working in MMIO mode.
However, I have problems getting this to work in XIP mode.
The flash chip has different register format for status access (it requires additional status address byte), it's also missing QE bits etc.
I like to have this in XIP mode, so I can do DMA transfers with little CPU interventions
Has anyone used a compatible NAND flash, preferably >1Gbit size and have it working in XIP mode?
Thanks
Show LessI upgrade my EZ-USB SDK to 1.3.4 today , but it makes my code can not work any more.
where can i download the old version of 1.3.
thanks a lot !
Show LessI am using an external RF power amplifier SKY66111-11 which uses two control lines CTX and CRX to switch from TX to RX,
I have seen some code which is confusing me see below.
I am using P2-7 for the CTX and P2-6 for the CRX
To transmit CTX = 1 and CRX = 0;
To receive CTX = 0 and CRX = 1;
To standby CTX = 0 and CRX = 0;
The queastion is how do I control the SKY66111-11 from the link layer?
#if
TX_RX_GPIO_ENABLE
*(uint32*)(CYREG_RADIO_TX_RX_MUX_REGISTER)&= ~RADIO_TX_RX_MUX_MASK; /* Clear Previous mux selection */
*(uint32*)(CYREG_RADIO_TX_RX_MUX_REGISTER) |= BLESS_MUX_INPUT_MASK; /* Set BLESS as the source of the mux */
*(uint32*)(CYREG_BLE_BLESS_RF_CONFIG) |= RADIO_TX_RX_SEL; /* Select Tx enable & Rx enable signals from BLESS as input to mux */
#endif /* End of #if TX_RX_GPIO_ENABLE */
Show LessHi,
I need to know do cypress has any EOL slated for CYPD-3120 and CYPD-3125 chipset. Do we have any latest SDK got released.
With installation of 3.3 creator, i faced some issue with SDK project(Version 3.0.2, April 10, 2017) it says above platform is no more supported. Pl confirm we already selected the chipset for our solutions and its almost into production.
Thank you,
Arun
Show LessHi,
I am a newbie to use the FX3 series USB controller.
I am now designing a product using the FX3s to communicate with PC and another special USB host device, which has a strict power limitation below 50 mA.
While attached to the special USB host, the speed is not important.
So I am now looking for every possible way from hardware design to firmware implementation to reduce the power consumption.
Would force the FX3 enter USB 2.0 high speed mode help to reduce the power consumption?
Would the crystal frequency selection between 19.2, 26, 38.4, and 52 MHz also affect the power consumption?
Any other suggestions are more than welcomed.
Thanks,
Jay
Show LessThe problem is that I can't find the handler (is that NMI_handler?) when brown-out detected.
Show Less
//Enable power monitoring control register for brown-out detection.
XMC_SCU_POWER_EnableMonitor(0x01, 0x80);
//enable a trap source
XMC_SCU_TRAP_Enable(0X20);
I do not have a pulse at the WaveDAC8 outputs wc1 or wc2 after the value table is done. I reduced the problem to the Project ‘2_WaveDAC8_TwoWaves’ from the example workspace AN69133. In this example, I measure a static sine as configured in waveform 1 at the output. I also routed signal wc1 to a pin to observe with an oscilloscope, there is no pulse.
My system :
CY8CKIT-059 (CY8C5888LTI-LP097)
PSoC Creator 4.2 (4.2.0.641)
OS Version: Windows 10 (Microsoft Windows NT 10.0.16299.0)
Show LessAs students of the University of Hasselt in Belgium, we are making a master thesis about Power Line Communication on low voltage DC (maximum 48V). Therefore, we are interested in the CY3275 Programmable Low Voltage Powerline Communication Development Kit. We would like to inform us about the availability and price. If this kit is not longer available, do you suggest any other options for us to use?
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023