All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
I would need to implement an emulation of hw flow control (rts/dtr) with USBUART (USBFS) module of CY8C3866LTI.
I see the fonction USBUART_GetLineControl() to "read" the emulated "pins", but I cannot find out how to "write" pins by software to let the PC know, for instance, that the PSoC "uart" device is currently unavailable to receive more data.
How can I "write" to those emulated pins with the PSoC ?
Show LessDear Madam/Sir:
We attached BDAdriver_interrupt_working_current, but not sure how to compile it, Would you please kindly answer these question:
1、what is the compile enviorment ? linux ?windows?
2、If it is linux enviorment, the Makefile can not work.
3、If it is windows enviorment, what is the IDE should be used to compile it?
Beside, would you please kindly give us a BDA driver guide for our ATSC tuner dongle?
Sincerely Thanks
Show LessIs there any documentation on accessing the HX3 configuration and/or attached i2C EEPROM from the upstream USB connection (the way that HX3 Blaster Plus does)?
Show LessHi,
I’m an embedded firmware engineer. I plan to use your MB9BF416R chip for our application development. Can you please give me a reference
Manual of that chip which can provide complete information on
how to use its memory and peripherals? For example, the detail description of
each CPU and peripheral register in order that I can configure each bit of them.
Thanks,
Show LessHi, Windows 7. WICED Studio 6.2.1
Unzipped installer. when I run it, regardless of where I choose to install IDE, it stops and tells me I do not have enough space. It claimes I have 1MB of space and need 1GB of space.
My C drive actually has 85GB of space and my F drive has 330GB of space. can someone guide me on how to solve this installation problem?
Show LessI am developing a bdc motor driver circuit.
I chosse 2EDL05N06PF parts.
Now i have a trouble,when use Signal generator test HO is normal,but use mcu pwm test HO is no output.
The details are as follows.
How can i to do next step? Thank you!
Show Less
Hi,
I am looking to attach cheap NAND flash via SMIF to PSOC6.
I was able to place a 1Gbit part from Winbond onto the PSOC evaluation kit and have it working in MMIO mode.
However, I have problems getting this to work in XIP mode.
The flash chip has different register format for status access (it requires additional status address byte), it's also missing QE bits etc.
I like to have this in XIP mode, so I can do DMA transfers with little CPU interventions
Has anyone used a compatible NAND flash, preferably >1Gbit size and have it working in XIP mode?
Thanks
Show LessI upgrade my EZ-USB SDK to 1.3.4 today , but it makes my code can not work any more.
where can i download the old version of 1.3.
thanks a lot !
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023