Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Product Forum Discussions

Browse the Community

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.

43902161 11153

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.

7619924 2696

Other Technologies

Discussion forum regarding Other Technologies including Power Management and Clocks topics.

753387 722

Recent discussions

Sort by:
jepaz
PSoC™ 4
I have been trying to export a Psoc4 Creator project into Keil uVision,  the export to v5 just didnt work at all, it seems uvision does not longer sup... Show More
JaVa_282241
PSoC™ 6
Hello, I would like to drive TFT 480x272/RGB/16bpp using PSoC 6.  The MCU provides "Graphic LCD Controller" component to do that, but it needs an exte... Show More
TechKoot
USB superspeed peripherals
Hello! Our project uses FX3 to transfer a large amounts of data using FX3. As we noticed, the real transfer speed from host PC to device is very low (... Show More
Yvan
USB superspeed peripherals

This sensor works well in RAW10, but when I use RAW8, it seems to have problems and the HSYNC signal is completely missing.

PSingh
LED Driver ICs

I am interfacing SPI module of SPC560DL40L3 microcntroller with TLE75008 to drive  5 relays.may i get some source or sample code for same.

YuTa_4942221
MOSFET (Si/SiC)
IPB720P15LMのシミュレーションモデルございますでしょうか? Webで確認した所、モデルがございませんでしたので、ご確認頂ければと思います。 【製品URL】 https://www.infineon.com/cms/en/product/power/mosfet/p-channel/ipb720p15lm/#!order... Show More
Kevin_Lo
USB superspeed peripherals
Dear Sir/Madam, Our customer engineers is using USBBulkSourceSink Example to test and get the UART debug log to acquire the error code to analyzer iss... Show More
_Tom_
Radar sensor
Hi  I use the position2go. I want to get raw data for 60 second. I revise and run extract_raw_data.m to finish it.But the total amount of raw data is ... Show More
amritsingh
PSoC™ 5, 3 & 1
Hi, I have been looking for PSoC 5 par number CY8C5868AXI-LP035 for months now. It is not available anywhere. Can someone help me find its stock (arou... Show More
Anna-xuan
Radar sensor
Dear friends,i  want to realize the funtion of  people counting  at a  place  with 60GHZ mmwave sensor,but i can't find any information about  it at t... Show More
Category Information

Product

Microcontrollers (MCUs), PSoC, Memory, Automotive, USB, Wireless and Other Technologies.