All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
text.format{('custom.tabs.no.results')}
Taking IPB017N10N5 as an example, there are few parameters about the diode in parallel and there are no descriptions about the diode reverse recovery current limit, diode shutdown device maximum power limit and SOA, where can I get this part of information? Where can I get this part of information?
Show Less你好,我想问一下,串口如果使用DMA模式的话,有什么方法可以让我获得串口接收到的数据,除了函数getbuffer以及DMA通道回调事件触发的时候能够获得其handle的buffer。这两种方法虽然可以得到串口收到的数据,但是如果之前配置的缓存区没有满的话,我们是拿不到buffer,因此也拿不到他的数据。
此外,我也用了CyU3PDmaChannelSetWrapUp函数,能够在DMA通道缓存区未满时将其强制提交,从而获得缓存区。这个方法虽然好,但是我用一个线程任务专门执行这个函数,它竟然有次数限制,当超过了某一个次数的时候,它就不再使用,这是怎么回事呢?
Hello,
We are developing the bootloader for the Infineon TC377 board. For that, we need the preserved RAM (The memory that shouldn't be initialized with zero during the controller reset) to hold the flag. So, we tried the keywords below for No-initialization and location, but AURIX is not supporting these keywords. Instead of the below keywords, what can be used to create the memory in the RAM, so that it shouldn't be modified after reset of the microcontroller.
#pragma NOINIT(BootMode_InPreservedRAM)
#pragma LOCATION(BootMode_InPreservedRAM,0x50000000)
/*Here first we are creating the variable BootMode_InPreservedRAM as no initialization and giving the address as 0x50000000 for LOCATION*/
Thanks in advance.
Show LessHello everyone, my board needs to use a SmartPIM1 series IGBT module: FP35R12U1T4, according to the SmartPIM1 assembly instructions AN2009_09, PCB boards have a layer of tin after the metalization of the aperture, I would like to ask this layer of tin is plated with the surface treatment using the sinking tin process? It seems that most PCB manufacturers nowadays are spraying tin, and there seems to be only copper on the inside of the holes, will this affect the assembly?
Another problem is that according to the assembly instructions the board needs to be drilled between 1.12mm ~ 1.15mm, I can find the best precision factory crimp hole hole diameter tolerance is also ± 0.05mm, it seems not quite able to meet the error requirements. I would like to ask you to play this kind of board to find what manufacturers to meet the requirements?
Show LessThere is said that this bright feet + logo a bit unlike is IR Mexico factory production, I can not judge, please gods look at, this is not authentic, thank you!
Show LessHi infineon
As the title said, I got a problem with "Vddk", I use the next formula to configure "Vddk", but some products(not all, same program) will exceed the threshold(±2%) when ambient temperature increasing, and the calculated value close to low boundary? Could you give me some advise? Thanks
Show Less
Hello,
we ported the wifi stack in our new product, it has a WiFi stability issue, mainly it shows SDIO bus communication error, we made a restart stack when it happened but we don't know where is the root cause, can you help us with this?
Thank you very much!
- setup
- pack: https://github.com/Infineon/AIROC-Wi-Fi-Bluetooth-STM32
- module/chipset: COMPONENT_4373/COMPONENT_MURATA-2AE
- after connecting to AP, send a request to fetch RSSI every 5 seconds
- WHD/WCM logging enabled
- host MCU:STM32H7B3LI, interface by SDIO
- RTOS: ThreadX
- issue
- got an error on "SDIO bus failed to come up , whd_kso_enable failed" from time to time, sometimes shows up just after connecting to AP, and sometimes happens a few minutes after
- few changes from the stack but no improvement:
- force speed as 25MHz ( not jump to 50MHz)
- force to use memory copy to internal RAM for DMA () -- bool "use_temp_dma_buffer = true"
- #define CYBSP_WIFI_SDIO_NEEDS_INIT (0)
- some timing/retry change to long
- #define SDIO_ENUMERATION_TRIES (1000)
#define SDIO_RETRY_DELAY_MS (2)
#define SDIO_BUS_LEVEL_MAX_RETRIES (200) - #define SPINWAIT_POLL_PERIOD 20
- #define KSO_WAIT_MS (2)
#define MAX_KSO_ATTEMPTS (1000)
- #define SDIO_ENUMERATION_TRIES (1000)
HI
Purchasing S29GL01GT11FHIV10 product, I would like to confirm why the silkscreen is not reflected in the complete, in the specification did not see this information. Attached is a complete picture of the product, please help to answer the question, thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/Nor-Flash/%E4%B8%9D%E5%8D%B0%E7%A1%AE%E8%AE%A4/td-p/736508
Show LessI am trying to use the BLCD Shield. I am unable to update setparameter(), which led me down the rabbit hole of downloading Kiel uvision5, buying a j-link mini and trying to install Config Wizard, all in order to fix the setparameter() issue which seems to still persist on the BLCD Shield platform, 2 years after being first identified.
my current roadblock is the downloading of the Config Wizard 1.x at https://infineoncommunity.com/2018Aug_GLOB_ATV_GATED_Config_Wizard_Id1003. I filled out the information and was emailed a link for downloading the software as well as other links. No link works. I would really like to get this working (with the ultimate goal, to run a motor using the BLDC Shield through an arduino. Any help would be appreciated.
Hi,
I have a AURIX MotorControl Application Kit with TC234LF, I want to switch from ADS to Visual Studio Code. I'm going to make it through the GCC compiler, but there is a problem using the winIDEA debugger. WinIDEA requires a license. I did not find a price list on the website and how to buy it.
Are there alternative debuggers that can be used in Visual Studio Code?
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023