All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
SPI flash memory MT25QL128ABA1EW7-0SIT works well for FX3 SPI booting. When I used it for CX3 SPI booting, I am not able to let CX3 boot from SPI flash memory. PMODE pins configuration has been confirmed. Using control center utility tool, firmware image file can be written to MT25QL128ABA1EW7-0SIT successfully. But can't boot from it. it is still enumerated as boot loader device, which means it failed SPI booting. May I know the difference between CX3 and FX3 in terms of SPI booting? Thank you.
Show LessI am using Application Kit TC3X7 V2.0 TFT board
I have configured BMHD but the board all the time boots from Internal flash ignoring BMHD settings
If i want to use Alternate Boot Mode or BMI to boot , which all changes i need to do on the board?
Show LessHi,
I am using CY8C6245LQI-S3D42 and I used the DFU examples to boot the system and created the application to run on AM4 core and everything is working well.
I wait for 5 sec in DFU to check if there is any updates or just move with the Application code.
I find that sometimes the device stops booting once in a blue moon. Now If I flash again just the boot loader, everything is fine , I need not have to write the Application, it moves from DFU in 5 sec to application.
I believe, there is some how the flash/DFU is getting corrupted. I want to protect this scenario. Can some one share how do I protect my DFU so that it never erases . Any example's will be appreciable, I am using USB CDC transport in DFU.
Regards,
Madhav
Show LessHello, World!
I am trying to install ModusToolbox and am getting the error message
Error: Failed to Login: "Network Error occurred": 'ContentNotFoundError'
Steps to reproduce:
1) Download and install the developer center launcher
2) Launch ModuxToolbox Setup
At this point the software gives the error message
At this point, it doesn't matter if I click "Login" or click on "ModusToolbox Tools Package". Login doesn't even ask me for a username. I get the same error message and "Next >" never becomes enabled.
Any help would be appreciated.
Show LessHello.
I'm planning to work with the CYUSB3KIT-003.
Reading and following the Kit User Guide, I am able to complete section 2.1 FX3 SDK Installation using the file ezusbfx3sdk_1.3.5_Windows_x32-x64.
Then next step, 2.4 Superspeed explorer kit installation, is the one not being able to complete. I am using the file SuperSpeedExplorerKitSetup_RevSS obtained from the CYUSB3KIT-003 design support section.
The installation stops and an error shows up. After clicking "OK " it rolls-back the installation of the items completed.
I would like to get directions to solve this. Its not clear what item is the one that supposedly found a newer version already installed. Anyways, this is right after installing the FX3 SDK, then probably this packet has something newer than the otehr installation is not expecting.
*I tried using the other file available: SuperSpeedExplorerSetupOnlyPackage_RevSS; this one is able to get installed, but then, following the user guide the next step is to use the update manager but this one can not be found, it seems this different package for the Superspeed explorer kit doesn't include that and other things.
Thank you,
Alan.
Show Less
Hello,
I am trying to flash littlefs filesystem on the qspi external serial flash memory in XMC7100 V1.1. As I see library mtb-littlefs is not included in the XMC7100 kit but i have included the mtb-littlefs from PSoc6 Kit to my project and in makefile included target as XMC7100 (my board).
BOARD: XMC7100 EVK Lite v1.1
Memory: External QSPI flash memory
These are the errors when I try to builld the file:
Initializing build: mtb-example-psoc6-filesystem-littlefs-freertos Debug APP_KIT_XMC71_EVK_LITE_V1 GCC_ARM
Prebuild operations complete
Auto-discovery in progress...
Auto-discovery complete
Commencing build operations...
Tools Directory: C:/Users/Prasad/ModusToolbox/tools_3.2
"Using linker bsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/COMPONENT_/TOOLCHAIN_GCC_ARM/linker.ld"
Constructing build rules...
Build rules construction complete
==============================================================================
= Building application =
==============================================================================
Generating compilation database file...
-> ./build/compile_commands.json
Compilation database file generation complete
Building 223 file(s)
Compiling ../mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.c -DCOMPONENT_APP_KIT_XMC71_EVK_LITE_V1 -DCOMPONENT_CAT1 -DCOMPONENT_CAT1C -DCOMPONENT_CAT1C4M -DCOMPONENT_CM7 -DCOMPONENT_CM7_0 -DCOMPONENT_Debug -DCOMPONENT_FREERTOS -DCOMPONENT_GCC_ARM -DCOMPONENT_MW_ABSTRACTION_RTOS -DCOMPONENT_MW_CAT1CM0P -DCOMPONENT_MW_CLIB_SUPPORT -DCOMPONENT_MW_CMSIS -DCOMPONENT_MW_CORE_LIB -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_FREERTOS -DCOMPONENT_MW_MTB_HAL_CAT1 -DCOMPONENT_MW_MTB_LITTLEFS -DCOMPONENT_MW_MTB_PDL_CAT1 -DCOMPONENT_MW_RECIPE_MAKE_CAT1C -DCOMPONENT_MW_RETARGET_IO -DCOMPONENT_RTOS_AWARE -DCOMPONENT_SOFTFP -DCOMPONENT_XMC7x_CM0P_SLEEP -DCORE_NAME_CM7_0=1 -DCY_APPNAME_mtb_example_psoc6_filesystem_littlefs_freertos -DCY_RETARGET_IO_CONVERT_LF_TO_CRLF -DCY_SUPPORTS_DEVICE_VALIDATION -DCY_TARGET_BOARD=APP_KIT_XMC71_EVK_LITE_V1 -DCY_USING_HAL -DDEBUG -DLFS_THREADSAFE -DTARGET_APP_KIT_XMC71_EVK_LITE_V1 -DXMC7100D_F176K4160 -I. -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1 -Ibsps -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/config/GeneratedSource -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/config -Ilibs/abstraction-rtos/include -Ilibs/abstraction-rtos -Ilibs/abstraction-rtos/include/COMPONENT_FREERTOS -Ilibs/cat1cm0p/COMPONENT_CAT1C -Ilibs/cat1cm0p -Ilibs/clib-support -Ilibs/clib-support/TOOLCHAIN_GCC_ARM -Ilibs/cmsis/Core/Include -Ilibs/cmsis/Core -Ilibs/cmsis -Ilibs/core-lib/include -Ilibs/core-lib -Ilibs/freertos/Source/include -Ilibs/freertos/Source -Ilibs/freertos -Ilibs/freertos/Source/portable/COMPONENT_CM7 -Ilibs/freertos/Source/portable -Ilibs/freertos/Source/portable/COMPONENT_CM7/TOOLCHAIN_GCC_ARM -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include/pin_packages -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C -Ilibs/mtb-hal-cat1 -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include/triggers -Ilibs/mtb-hal-cat1/include -Ilibs/mtb-hal-cat1/include_pvt -Ilibs/mtb-hal-cat1/source -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C/include -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C -Ilibs/mtb-pdl-cat1/devices -Ilibs/mtb-pdl-cat1 -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C/include/ip -Ilibs/mtb-pdl-cat1/drivers/include -Ilibs/mtb-pdl-cat1/drivers -Ilibs/mtb-pdl-cat1/drivers/third_party/ethernet/include -Ilibs/mtb-pdl-cat1/drivers/third_party/ethernet -Ilibs/mtb-pdl-cat1/drivers/third_party -Ilibs/retarget-io -I../mtb_shared/mtb-littlefs/latest-v2.X/bd -I../mtb_shared/mtb-littlefs/latest-v2.X -I../mtb_shared/mtb-littlefs/latest-v2.X/include
../mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.c:487:5: error: 'cy_stc_smif_mem_device_cfg_t' has no member named 'mergeTimeout'
487 | .mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE
| ^
make[1]: *** [libs/core-make/make/core/build.mk:283: C:/Users/Prasad/mtw/Littlefs_Filesystem/Littlefs_Filesystem/build/APP_KIT_XMC71_EVK_LITE_V1/Debug/ext/mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.o] Error 1
make: *** [libs/core-make/make/core/main.mk:385: secondstage_build] Error 2
"C:/Users/Prasad/ModusToolbox/tools_3.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=C:/Users/Prasad/ModusToolbox/tools_3.2 CY_IDE_BT_TOOLS_DIR= -j8 --output-sync all" terminated with exit code 2. Build might be incomplete.
When I comment the line:
#if (CY_IP_MXSMIF_VERSION >= 2)
/** Continuous transfer merge timeout.
* After this period the memory device is deselected. A later transfer, even from a
* continuous address, starts with the overhead phases (command, address, mode, dummy cycles).
* This configuration parameter is available for CAT1B devices. */
//.mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE
#endif /* CY_IP_MXSMIF_VERSION */
I get failed to creat spi device block:
Could someone help me with ".mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE" error?
When using the mtb-littlefs through the mtb-shared, how do I enable the cy_hal, freertos and thread in make file?
I tried to add the necessary comments on my application makefile but it is not enabling the corresponding if condition in the files in mtb-shared folder/mtb-littlefs!
best regard,
PrasadA
Show Less
Hello everyone! Is it possible to directly measure the current running through a DC motor using the BTN9970LV shield? I tried finding the answer in the data sheet and user manual but I was unable to. Thanks for your responses!
Show LessI am trying to load the cyfxuvcinmem_bulk example on my SuperSpeed explorer kit however once I upload the firmware to RAM or I2C, the device does not enumerate as a UVC camera on my laptop. When I last tried a year or so ago, it did work. Is there any known modifications or issues that would prevent the device from enumerating? I am using the cyfxuvcinmem_bulk example taken straight from `<FX3 SDK Install>\firmware\uvc_examples\cyfxuvcinmem_bulk` with no modifications. If I load the LED blink example, the board works as expected.
Show LessHello everyone,
I'm experiencing difficulties installing the KitProg Programmer drivers on my system running Windows 11. Each time I attempt to install, Windows fails to find the appropriate drivers for the device, as illustrated in the attached screenshot. I've attempted the usual methods such as searching for updated drivers through Windows Update, but to no avail.
Could someone guide me on how to properly install the KitProg Programmer on a Windows 11 system, or provide a link to the specific drivers required? Your assistance would be greatly appreciated to resolve this situation.
Thank you!
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023