Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Product Forum Discussions

Browse the Community

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.

43742667 11140

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.

7596635 2689

Other Technologies

Discussion forum regarding Other Technologies including Power Management and Clocks topics.

750946 722

Recent discussions

Sort by:
SoU_4942226
MOSFET (Si/SiC)
シングルパルスの場合、パルス幅はグラフにあるとおり100us, 1ms, 10msの時間ONさせていると思いますが、OFF時間についてはどのように考えればよろしいですか?(OFF時間をどれだけあければ次のパルスをシングルパルスとして扱っても良いですか?)スイッチング電源の場合、FETを周期的にON/... Show More
Venkatesh
TRAVEO™ T2G
Hi All, What's the difference between Body High and Body Entry Traveo II chips. Is CYT2BL5 is a Body entry / Body High Chip? If any document provides ... Show More
TaOn_4865801
MOSFET (Si/SiC)
下記のMOSFETについて、ボンディングワイヤーの材質を教えてください
IPLK60R360PFD7
lixia
Class D Audio Amplifier IC
About "CSD"
Solved
Hi @Liz I have an idea, do not know whether it is feasible, my purpose is as follows: 1, the capacitor CT is set to 47uf-68uf, the purpose is when ove... Show More
RajivB
XMC™
Any example from Infineon to show how ADC DMA event handler can be  inside a Thread task in XMC4500 MCU assuming FreeRTOS is used as the multi threade... Show More
e_moir
MOSFET (Si/SiC)
Hello, 1.  Output filter MG10000850 (Designator: L2). The specified value of the inductance in the document MG10000850 is different from the circuit. Show More
yangyong
PSoC™ 4
AMUXBUS
Solved
Both  adc and capsese  have AMUXBUS,  Whether the AMUXBUS is the same.  When using AMUXBUS in ADC and Capsense at the same time, will  interfere with ... Show More
ankitvats846
USB superspeed peripherals
Hi,  FPGA generates interrupt signal to FX3 through GPIO.  Fx3 receives the interrupt signal. For capture interrupt in FX3, I refer this example Firmw... Show More
NamDo
AURIX™
Hello everyone,  I have the AURIX TC387 Motor Control Application Kit. I also have access to the source code of the demo project downloaded from The D... Show More
Sylvia
USB superspeed peripherals
Hi,  I implement a UVC/UAC firmware. We should install driver like this thread. Otherwise, the video and audio can not be played. I want to ask is it ... Show More
Category Information

Product

Microcontrollers (MCUs), PSoC, Memory, Automotive, USB, Wireless and Other Technologies.