All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
I would like to know, whether the TC297 support Linux operation system or not? Why?
Thank you for your help,
Best regards
Lucas
#8042000 12467 Show Less
Greetings- I have a PSoC5 design in Creator 4.3 with 2 1/2 Duplex RS-485 Uarts. They were 1st placed with internal clocks @ 9600Baud.
We need to change bit rates periodically during execution, so I changed the UART configurations for external clocks and added the clock components as customary. The design built fine, but never again. Any attempts to change either UARTS configuration now will fail to build, with "can't fit into 24 UDB blocks", and the sjplacer.exe failure (0x0000000B). Even reverting the schematic back to internal UART clocks, and deleting the clock components will cause the builder to fail.
Enough resources were available for the first build. I don't think they are getting released when no-longer needed by the design. We are tracking changes with GIT, and there seems to be an increasing number of keys being created, but very seldom see them deleted (only tagged as visible false)
"Clean and Build" does not fix this.@
Thanks
Ken Ayre/Sielox
Show LessDear sir,
I want to compile Windows MeshClient app source code, but there is a error report ---- the directory of WICED-Studio-6.4\common\libraries\mesh_core_lib or WICED-Studio-6.6\common\libraries\mesh_core_lib doesn't exsist. Please help to solve this problem. Thank you.
Show LessInfineon lists only PCoC 4 products on their webpage.
I want to use PSoC 5LP and specifically CY8C5888AXI-LP096.
Does Infineon plan to dump all but PSoC 4 ??????
Show LessI'm working on a PsoC5lp board with PsoC creator 4.4 . My project is fairly due to the driver for my I2C display that my school is making me use. I set the heap size to 200 bytes. I set "use newlib-nano" to true. I set "newlib-nano float formatting" to true ( -u _printf_float). I also set link time optimization to true and and optimization level to size because of the aforementioned driver.
When I use sprintf on any non-zero float, the stringbuffer contains the following three values in place of the float:
0x00 '\000'
0x2E '.'
0x80 '\200'
The code I use is fairly simple and equivalent to:
char stringbuffer[20];
sprintf(stringbuffer, "(%.1f, %.1f)", 1.1, 1.1);
What is going wrong? I saw on stackoverflow that there might be a bug in the linker script... but that goes way above my head.
https://stackoverflow.com/questions/28746062/snprintf-prints-garbage-floats-with-newlib-nano
Show LessI am looking for the samples of CY8C5888AXI-LP096 chips for our new project. I sent an email to customercare@cypress.com
and also to German sales office but no response.
Who to contact for samples in Slovakia, please ?
Show LessHi Sir,
When using P6/P4/P4BLE development is complete.
Our product starts mass production, what tools are used to download the program?Make the production process
convenient and fast;
Best regards,
Robin
Show LessHi,
In a design I need to connect a MIPI camera to CYUSB3064 for getting the USB3 signal out to the PC through a USB-C connector. I realize that the CYUSB3064 needs also USB2 signals, DM&DP. I also need the DM&DP to connect to my processor. Is attached schematics a possible way to go forward for these connections? Could someone see if having the USB2 signals through a HUB would be an issue?
/Thanks in Advance.
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023