All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
text.format{('custom.tabs.no.results')}
Hello
I am doing a CX3 UVC configuration and I want to configure MODE6 according to IMX294 datasheet as shown below.
I would like to know what values I should set for H-Active, V-Active, H-Blanking, V-blanking?
Do I need to make changes to the CSI Clock values?
Best Regards,
Yaqi
Show Less
By using EZ USB suite and utility I have created one of the configuration for the OV5640 image sensor. But when I built the project, I'm getting the error "cycx3gpifwaveform.h file not found."
In the comment, it is mention that "Get the header file from CY Tech Support and add it to the project."
This will be a generic file or the specific one?
How can I get hold of this file?
I have tried contacting CY team through email.
Show LessDevice application is HDMI input to the USB output
The design is based on the lattice USB3 Video bridge development kit. I am able to stream the video properly using amcap on windows os.
But when I am trying to stream the video using GStreamer application on Linux. It receives one frame and then the application stops.
The firmware I am using was given by the lattice.
what modification I have to do to make it work in Linux also?
Show LessHi,
How do I generate checksum in WICED studio? I know in PSoC Creator, the checksum is stored at the address 0x9030 0000. Is there something similar on WICED Studio?
Thanks!
Show LessHello,
We are moving from the cymdhd driver to the brcfmac backport with an CYM43455. We needed to set the following dhd build flags in order to achieve good 5Ghz WiFi throughput. What are the equivalent settings in brcmfmac?
DHDCFLAGS += -DCUSTOM_AMPDU_MPDU=16
DHDCFLAGS += -DCUSTOM_AMPDU_BA_WSIZE=64
DHDCFLAGS += -DCUSTOM_GLOM_SETTING=8
DHDCFLAGS += -DBCMSDIOH_TXGLOM -DCUSTOM_TXGLOM=1
DHDCFLAGS += -DDHDTCPACK_SUPPRESS
DHDCFLAGS += -DRXFRAME_THREAD
DHDCFLAGS += -DCUSTOM_MAX_TXGLOM_SIZE=31
DHDCFLAGS += -DMAX_HDR_READ=128
DHDCFLAGS += -DDHD_FIRSTREAD=128
Thanks!
Show LessHello
I have problem with Quicksilver IoT Development Kit.
Do you have information how build example program for this MCU?
When I click Build 'Defaul' for project 43xxx_Wi-Fi
I have this communicat:
Can sameone please take the time and showe me how to compile example program for this board and how upload for the MCU.
I have this version of Wiced:
Best Regards,
StaryAnoda
Show Less
Hi,
We are working with the LAIRD-EWB module that use CYW4343W (wifi - BLE combo) with a STM32F412. We want to use the Quad SPI on the MCU but there is no qspi platform related to STM32F4xx in Wiced (WICED/platform/MCU/STM32F4xx/peripherals).
Is there a way to have access to stm32f4x_qspi Library ? What would be the best way to do it and if there's any exemple to use the stm qspi library.
1. Create a platform like the one in the stm32L4. If it's possible, is there any guideline ?
2. Include the STM library and use it directly in my application file like I would do it in STMCube ide.
For information, we want to use the quad spi to store data in a PSRAM. Any help, could be usefull.
Thank you
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023