Product Forum Discussions
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Recent discussions
Hello,
in BLE component is Custom characteristics "MESSAGE" and in Properties are two parameters: Read and Write.
These parameters I can change by "tick" button in configure window. It's clear.
But how I can enable/disable for example Write parameter directly in C file?
I would like to have something as:
if ( i == 1) "Write is enable"
else "Write is disable"
Thanks in advance, Libor
Show LessHi,
I have a question When is try to build the firmwarer for FX2LP using keil uVision2.
The build result is shown attached pic.
I can’t find the exit-code =4
also, I don’t know what is means
could you give me solve or advice about this problem.
My dev system base on windows10, and I try also windows7 dev system too. But it’s result same.
Show LessDoes somebody know what is the size of the marked area on attached picture? I found some dimensions shown on 2nd attached picture but I couldn't find that one.
Show LessI bought a FM4 S6E2C-Series Pioneer Kit. I installed the Serial Port Viewer Software and the CMSIS-DAP firmware package. When I launch the Serial Port Viewer, a little window pops up and then in a few seconds disappears. I running Windows 10. Anybody have any suggestions?
Show LessHi everyone,
I bought Solar-Powered IoT Device Kit recently.
Is there a way to attach an antenna to the BLE transmitter of that kit to amplify the signal?
I've tried simple parabolic reflector after googling but that was not enough.
Thanks in advance.
vijay
Show LessI don't know output of data where from the q port of filter how to communicate with the bluetooth .How to configure parameters between them.
Show LessHi to all.
It's quite possible that we will go with mass production of boards with cyble022001 module on them.
Does anyone have some experience with this kind of thing? What to use as a programmer, how to connect it with the jig, how to organize test firmware on the BLE module?
Any kind of practical advice would be great, or pointer to the place where I can find more data on this, regarding the Cypress BLE modules.
Thanks
Show Less