All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
Hi,
I've cloned project from github from this link : https://bitbucket.vih.infineon.com/projects/CCSESS/repos/mtb-example-anycloud-mqtt-client-optiga/browse but when I try to debug or run the file then it says error with command: gdb --version . So how do i fix this? I've also referred to this link: https://community.cypress.com/t5/Wireless/Error-with-command-gdb-version/m-p/267766 but since device are different and I also dont use wiced studio instead I use modus toolbox v2.2. so did not understand properly .
Please kindly help.
Regards,
Soram
Show LessA 1 Mbit SPI FRAM (FM25V10-G) appears identical to a 1 Mbit SPI nvSRAM (CY14V101Q3-SFXI) from a user perspective.
What are the key differences between these technologies?
For which applications would one be preferred over the other?
Are they interchangeable in a design?
Greg
Show LessShould the minimum RESET# pulse width at power on be measured using Vil or measured using Vih?
We are using the CX3 (CYUSB3065-BZXI) for a SPI Receiver design, where it is operating as the SPI master and receiving 8/16-bit samples which are being automatically DMA'ed to USB within the device. When the design works it works well - with the 8/16 bit data properly aligned. However after subsequent clean SPI restarts (with full SPI re-initialisation), we may, or may not, be byte/word aligned. We have deliberately sent known data, to prove where the problem lies, and have confirmed the SPI data is properly aligned from the transmitter to the CX3 receiver. However, somehow the CX3 receiver seems to be incorporating a 2, 4 or 6bit offset into the data received. Once the data stream is started is DMA'ed directly so all data has this same offset. Also by way of debug, changing some ms delays around the SPI restart seems to alter (improve) the alignment success rate.
Is there any CX3 Errata with the SPI receiver DMA relating to bit alignment?
Your assistance would be appreciated.
Hello.
Tool: Modustoolbox 2.2
Target: CYBT-413055-02
How can I avoid build error with "undefined reference". I do need "snprintf".
I add #include "stdio.h". What library do I have to add?
Show Less
I have just bought a CYBT-353027-EVAL board, and I have installed WICED Studio.
This page says "Paste the folder in the WICED Studio 6.2 folder path …\ WICED-Studio-6.2\20706-A2_Bluetooth\Platforms\", but this path does not exist on my PC.
I downloaded "ez_serial_cybt_353027_fw_image_1.2.27.27", but I can't find instructions on how to install it.
Can anyone advise on the next step? Thanks.
Show LessI wish to debug a legacy board using a MB96F637RB processor to do some reverse engineering and modification of existing code. MY plan was to use a MB2198-01 Emulator with Softune workbench 6, however I cannot find library files that support the CY/MB96F637RB processor. Any help would be appreciated including suggestions about other approaches.
Show LessI have a Vision Display graphic lcd, it uses UC1701 driver I think it supported in GUIDRV_SPage. CE223726 has an example on how to use the emWin using a different lcd. Page 6 of CE223726 doc shows how to add emWin library to PSoC Creator, I do not see this option on mine. I'm using CY8CKIT-062-BLE and have installed the complete setup for the kit.
Questions:
- Is there anything I have to install to show the graphic option?
- Does PSoC supply GUIDRV_SPage driver?
- Has anyone used this DOGS102-6 LCD? Share example codes?
I appreciate any help or pointer. Thanks.
Show LessDear Sirs,
I am not able to compile my current project (TARGET:CYBT-413055-EVAL) anymore - no idea why. When building the following message occurs:
/bin/bash: g++: command not found
make[1]: *** [../mtb_shared/core-make/release-v1.5.0/make/core/build.mk:376: C:/Users/Achim/mtw/PFSLocatoriAP2/build/CYBT-413055-EVAL/Debug/.metadata/.plugins/org.eclipse.cdt.make.core/specs.o] Error 127
make[1]: *** Waiting for unfinished jobs....
make: *** [../mtb_shared/core-make/release-v1.5.0/make/core/main.mk:414: secondstage_build] Error 2
In the same IDE I have the "Empty_BTSDK_App". which is running through fine.
Show Less
I am getting frequent debugger crashes, while debugging my PSoC creator project. I am using a MiniProg4 programmer.
Environment:
PSoC Creator 4.4 (4.4.0.80)
Culture: English (United States)
OS Version: Microsoft Windows NT 6.1.7601 Service Pack 1
CLR Version: 4.0.30319.42000
MiniProg4 Firmware:
MiniProg4. CMSIS-DAP Version 2.0.0. Firmware Version 2.10.878. Hardware Id 05.
This is happening frequently, whether I'm stepping-through code, or just hitting breakpoints.
Let me know what other information I can provide that would be useful in solving this
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023