All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
Hello.
I have fwDownload.exe running on Windows to configure in production CY7C65213-32LTXI.
I need now this tool to integrate on Linux?. Is it available?.
Thanks
Hi,
I am using a CYW43012 (Murata LBEE59B1LV) with LPC56407 on a dedicated PCB. I try to set up the WiFi by creating Access Point or scanning local networks to verify the hardware.
At the moment I can reliably communicate with the module using SDIO and enable functions 1 and 2. I can read the state of those functions - function 1 is enabled and ready, function 2 is enabled but not ready.
I have found an example code for RT1170 and CYW4343W using the same initialization protocol. In this example during initialization there is a part of writing firmware for WiFi.
My question are:
- do I need Function 2 ready to scan WiFi or create Access Point?
- do I need to write WiFi firmware to the CYW43012 before scanning WiFi or creating Access Point?
Thanks,
Piotr
Show Less
i am using multiple CYUSB3324 in cascading. For an example if i am using 2 HUBs in cascade, in this cascading 2nd hub's upstream is connected to the downstream of first hub and first hub is connected to HOST. if my 2nd HUB goes in to the suspend state then will it also effect the 1st hub ? will first hub also go in to the suspend state ?
Show LessIs DMA of CYW54907 exposed for application development (such as for offloading CPU when transferring large amount of video data)?
I learned from previous post that DMA of CYW43907 was NOT exposed to application development.
Harris
Show Less
Hi.
I'm using CX3, and have I2c problem.
Hi,
The Device configurator in ModusToolbox can assign an INT signal PIN for SPI.
My questions are:
1. Is this INT signal PIN input or output for SPI?
2. If it is input, on what condition CYW20719B2 will receive this INT signal. And how to define interrupt service routine?
If it is output, on what condition CYW20719B2 will output INT signal?
Best regards
Jian
Show LessHello
I am trying to use the TDM in the I2S module but I can't find information in the datasheet about the TDM-A and TDM-B modes.
Are there any resources or test code available for the TDM on PSoC-6 ?
thanks
Show LessDear Sirs and Madams,
CyIntSetSysVector (4, & CySoftwareReset);
Is it possible to assign a reset function to the exception reserved as above?
Or something it should be noted there will be?
Regards,
Show LessHi there,
I'm using cyusb3014 FX3 usb IC for I2C/SPI/GPIO handling and it all works fine.
SPI is for flash control.
But SPI speed is little slow, so to increase SPI speed, increased clock from 8 to 32Mhz and reduced threadsleep time 10->1ms.
(From reference code - cyfxusbspidmamode.c)
Then SPI is more faster but still slow.
So I increased page size from 256 to 1024 byte then, speed more faster but some read/write data seemed corrupted.
looks like except 256 byte other data is all 0xFF.
Please let me know how to expand spi page size over 256 byte
or fix abnormal data bug.
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023