All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
Hello,
I am willing to order this product and have it in cart for two days now. I did not find any video on how to use the adapter board. I saw only one Document which state the pin configuration for (1,3 and so on) but still not able to get the idea on how to use this board. Retired board like AudioHub Nano is plug and play and a video is present online on how to use it. For the new Flex evaluation board only one page documentation is given and nothing else. Not sure where to connect these 1,3 pins? What microcontroller etc. nothing present. Please help so I can order it and use.
Show LessThis BTS7004-1EPP, the output is connected to the DC motor driver chip, and then to the motor, in that case, this RGND removed and directly grounded will work, right? Thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/7004%E6%8E%A5%E5%9C%B0/td-p/723932
Show Less
Hello
< I would have post again to correct mt TYPO, sorry.>
Customer intend to use BTS428L2 for next model.
Customer want to estimate BTS428L2 Nominal load current at Tc=60 deg-C.(not 85-deg-C)
In the data sheet of BTS428L2, ILoad=5,8A(MIN) at Tc=85 deg-C.
Customer let case temp 60deg-C, in order to increase load current ILoad=6.5A( this is customer's goal).
Anyway,
I had found application note below ** , and found Fig.36 Relative Rdson vs Tj.
I see Coeff = 71 at Tc= 85 deg-C. And also, Iload =5.8A(MIN).
I also see Coeff =61 at Tc=60 deg-C.
==>
Therefore, I think Iload at Tc=60 deg-C is,
So, Iload at 60degC is IL = 5.8A(85deg-C) / ( 61/71) = 6.75A.
Is this wrong?
I would have your advice.
Best Regards
****
Application Note: Smart High side switches
https://www.infineon.com/dgdl/Infineon-Application+Note-PROFET+12V-What+the+designer+should+know-AN-v01_00-EN.pdf?fileId=5546d46259b0420a0159d5c957260d9c
****
Are there available instructions or guidance on connecting the BGT60TR13C development kit to a jetson orin nano? Or a way to compile the sdk for the jetson? Following the "Building SDK from source code" in the RFS SDK Documentation in the radar_sdk didn't work for compile or install using python wheel.
Show LessHello everyone!
I am trying to use Example bgt60tr13c with Matlab 2017b. I have some problem when use demo:
>> MatlabWrapperExample
Incompatible MEX-file 'D:\Infineon\radar_sdk\libs\win32_x64\DeviceControlM.mexw64': Loading MEX file built by R2021b is not supported for this release.
Error in RadarDevice.get_version_full (line 187)
[ec, version] = DeviceControlM('get_version_full');
Error in MatlabWrapperExample (line 39)
disp(['Radar SDK Version: ' RadarDevice.get_version_full()]);
And when I try to build DeviceControlM.c:
>> mex -v CC=g++ -O -DSNPRINTF=snprintf -I'D:\Infineon\radar_sdk\sdk\c\' DeviceControlM.c
Error using mex
D:\Infineon\radar_sdk\sdk\matlab\RadarSDKMEXWrapper\DeviceControlM.c:56:46: fatal error: ../ContextWrapper/MWrapHelpers.h: No such file or directory
compilation terminated.
Could someone please help me resolve this error?
Show LessFrom a linux system, I want to read back the configured program image from a CYC65215 part and check that its CRC is correct -- assuming it has an appended CRC. Does the image have a CRC? Is the CRC generated using a known algorithm with a standard polynomial? If so, which polynomial?
Show LessHello, I would like to ask how to realize the real-time display of the speed, just like static_distance, for the FFT transform is not very clear inside the details, there is no sets of
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E9%9B%B7%E8%BE%BE%E4%BC%A0%E6%84%9F%E5%99%A8/On-the-issue-of-BGT60TR13C-real-time-display-speed/td-p/721701
Show Lessin TC38x,Can the local memory unit(LMU) and thre Distributed LMU (DLMU) as a whole LMU to be used in OVC function SAL-TC387QP-160F300S AD
Show Less你好
目前使用"UART_VCOM_1_KIT_TC397_TFT"範例在Triboard TC397上進行測試。
開啟兩組ASCLIN 模組0跟模組4並且在中斷設置中有更改相對應的向量表數值,進行以下交互測試:
1. CPU0_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(0)"跟進行輸出"Hello World!" ==> 可以正常顯示
2. CPU1_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(1)"跟進行輸出"Hello World!" ==> 無法顯示
3. CPU2_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(2)"跟進行輸出"Hello World!" ==> 可以正常顯示
4. CPU3_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(3)"跟進行輸出"Hello World!" ==> 可以正常顯示
想請問為何在CPU1_Main.c會有此問題?
#AURIX
#Tricore
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023