All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Featured Discussions
大家好。
TLE9879开发板,官方自带程序,调节速度使用电位器设定,电机能够正常工作。但是如果设定一个固定转速,比如Emo_SetRefSpeed(1000 ),那么电机启动的时候,需要用手转一下,电机才能够正常启动运转,否则就不转动。
已经试着调试过启动占空比,给定的速度,以及PID参数,都不管用。
问下能够得到指点一下,感谢!
Show Lesshi,Experts
I accidentally clicked “Solved” on the previous post,There is still this issue,Please help!
When I was debugging the two channel ASCLIN serial ports, I found that sometimes (with a high probability) when 275 ASCLIN receives data, the data length and received data may be messy, as shown in the following figure。
My software's purpose is to receive 8 bytes, then check the correctness of the data, and then return some data。
ASC_INIT ,the initialization function is shown in the following figure。
On the hardware side, I measured the waveforms when receiving correctly and when receiving incorrectly, and compared them to see that the waveforms are the same。May I ask where the problem is with the software?
best wishes
Show LessHi Infineon.
Below is sample code for DFU(device firmware upgrade).
https://github.com/Infineon/mtb-example-psoc4-dfu-basic
This sample code explains DFU using I2C or UART.
Is there any sample code for DFU using SPI?
Is my understand correct that PSoC4 can use SPI for DFU?
Or can only I2C or UART be used in DFU and not use SPI?
Best Regards.
YuMa
Show LessHello,
I am developing a program that executes the XMC Flasher .exe, and programs a board using said flasher.
However, I would like to be able to program/set BMI of multiple boards at the same time by having multiple programmers connected into my PC. If multiple XMC programmers are connected to my PC at once, is there a way to identify, select, and control a specific programmer, perhaps through the programmer's COM port or serial number?
If not possible through XMC Flasher, is there is other software that would accomplish what I'm trying to do?
Thank you,
Alex
Show LessHi,
My code was written on PC #1, a Intel-base Win11 system. I copied the code to PC#2, a virtual machine (Vmware fusion) running Windows 11 ARM Edition on MacBook M3.
Both PC#1 and PC#2 have PSOC Creator 4.4. When I do Project -> Update Components, the Component Update Tool shows incorrect version numbers on PC#2, while PC#1 shows the correct versions.
On PC#2 (ie, Win11 ARM):
A similar error was reported here: https://community.infineon.com/t5/PSoC-Creator-Designer/Unable-to-update-components/td-p/360176
Since PC#1 is getting the right versions, I suppose PSoC Creator Update Server is up and running.
I suspect that PSOC Creator 4.4 was built with the Intel version of the C++ library so the creator is not compatible with the Arm64 version. Can anyone confirm?
Additional info:
PC#1 has Microsoft Visual C++ 2015-2022 Redistributable (x64) - 14.32.31326 and Microsoft Visual C++ 2015-2022 Redistributable (x86) - 14.32.31326
PC#2 has Microsoft Visual C++ 2022 Redistributable (Arm64) - 14.30.30704
Thanks!!
--Tony
Show Less
1.TLE9879 _Evalkit_v1.4 What are the main functions of swdio R46 and swclk R50 and how are these values selected?
2.tle987x series power up swd part power up timing have a detailed explanation?
--------
Infineon-Z8F80032532_HW_Design_Guideline-ApplicationNotes
-----
Infineon-BLDC_shield-UserManual-v01_02-EN
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/SWD/td-p/716438
Show LessI own Rev11 of PSoC6 BLE PIONEER KIT.
What kind of support can I get?
Hi.
I use the CYBT-413061 module (CYW20721B2) on a custom board and try to run the RFCOMM_Serial_Port SPP demo in ModusToolbox 3.2. The code seems to load OK, but when starting the Client Control App and open the serial port, nothing happens - the controls are all greyed out. I then also run BTSpy and connects from a Windows 10 PC as suggested in the instructions - the Client Control App then seems to connect (not greyed out anymore), but nothing happens when pressing any buttons. BTSpy however, seems to display everything, like when hitting a key on Windows/TeraTerm BTSpy, it displays the messages - but nothing shows up on the Client Control App SPP tab or message window.
What could be wrong?
Regards, Roger
Show LessHi~
I'd like to import sameple application named 'Hello Sensor ' from based on CYW20706 to CYBT-343026-01
Because there is no sample applicaion which has same name in CYBT-343026-01
After installing sample application, I tried to exchange BSP from CYW20706 to CYBT-343026-01.
I found some decription indicates successful, But some otheres were not.
Operation is okay after build and flash. But I'm still curious whether it is really okay or not.
Please make me sure it
I attahced error code picture
Many thanks
BRs
Daniel Lim
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023