Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Pressure Sensors Forum Discussions

Sort by:
null_pointer
Pressure Sensors
各位好,我在使用dps368进行参数测量,目前温度测量是正常的,但是气压的变化数据实在过大(静止状态下),我想询问下论坛里有老师前辈们实现过手册中写到的2cm高度检测吗?目前英飞凌哪一款最适合动态情况下的gaos 我测量的高度大概都是在m级别变化,寄存器给的已经是最高精度的配置了。两块传感器,在同一... Show More
Kenta
Pressure Sensors
I am working on the pressure sensor (DPS310) for my study. The time resolution of the sensor is around 4Hz which I would like to develop. Do you guys ... Show More
ThongTran
Pressure Sensors
Structure of messages transmit (SP40T (SP400-15-11)) to receive (CMT 2219B)? How to read sensor values in SP40T(SP400-15-11) microcontroller? (temper... Show More
ThongTran
Pressure Sensors
Structure of messages transmit (SP40T (SP400-15-11)) to receive (CMT 2219B)? How to read sensor values in SP40T(SP400-15-11) microcontroller? (temper... Show More
Mitchell_shen
Pressure Sensors

In our factory, PCBA will go through water clean process.

Does Tire pressure sensor(TPMS) allow this clean process?

Hemn_87
Pressure Sensors
Hi Dears.I want to read parameter from sensor by sending command through out I2C for the SP370 (900 kPs) In programming Mode.I can read Temp and Volta... Show More
Edenmalka
Pressure Sensors
I need a barometric sensor, it must be waterproof, I see that the DPS368 is an option but I'd like to understand:   1.Is the sensor sensitive to water... Show More
Bellawu
Pressure Sensors

这是一位用户的咨询,希望帮忙解答,越详细越好,有图有真相,任何能辅助说明的文档或者视频资料都可以。

智能手环中一般都有哪些传感器,各自的作用是什么?英飞凌能提供哪些,具体的型号是什么?

Forum Information

Pressure Sensors

Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.