Pressure Sensors Forum Discussions
各位好,我在使用dps368进行参数测量,目前温度测量是正常的,但是气压的变化数据实在过大(静止状态下),我想询问下论坛里有老师前辈们实现过手册中写到的2cm高度检测吗?目前英飞凌哪一款最适合动态情况下的gaos
我测量的高度大概都是在m级别变化,寄存器给的已经是最高精度的配置了。两块传感器,在同一个位置同一个时间上电,差别也十分大,想知道导致这种变化的原因是什么?以及在运动过程中这个气压计实际的相对高度测量精度究竟能够达到多少?
谢谢各位!
Show LessIn our factory, PCBA will go through water clean process.
Does Tire pressure sensor(TPMS) allow this clean process?
这是一位用户的咨询,希望帮忙解答,越详细越好,有图有真相,任何能辅助说明的文档或者视频资料都可以。
智能手环中一般都有哪些传感器,各自的作用是什么?英飞凌能提供哪些,具体的型号是什么?
Hello everyone,
My name is Kirtan Soni and I am trying to interface the infineon's KP253 pressure sensor with the arduino mega. So far I have been able to get the output readings from the sensor (not what I need) and I think that I am using the correct SPI protocol as per give data sheet.
I am getting a diag1 error (As per datasheet) in my readings. I will explain what I did in depth below:
This is my circuit diagram. According to the datasheet the KP253 has a 16bit SPI transfer register the protocol is MSB first, 0.1 - 5 MHz clock speed, model 1. I have used the SPI.transfer16() to read and write to the register of the sensor, I am getting the readings and the readings are also changing with the rise and drop of temperature.
To check whether my connection and program is right I also write the identifier code and it gives me proper response as indicated in the datasheet.
This is the output I get by converting it to binary, I get - 0101000100110111 which is correct.
But when I write the temperature read command it gives me - 0101001011000110
So according to the response structure I get Diag1 error - 010
Here is my code:
#include<SPI.h> //Library for SPI
const int CS=4;
volatile int Response;
void setup (void)
{
Serial.begin(115200);
pinMode(CS,OUTPUT);
digitalWrite(CS,HIGH);
}
void loop(void)
{
digitalWrite(CS,LOW);
SPI.begin();
SPI.beginTransaction(SPISettings(4000000, MSBFIRST, SPI_MODE1));
Response = SPI.transfer16(0b0100000000000000);
SPI.end();
digitalWrite(CS,HIGH);
Serial.println(Response);
}
I tried everything that I knew but I don't know what am I doing wrong?
Thank you for your time.
I really appreciate your efforts.
To make your efforts a bit easy I am attaching the link to the datasheet as well.
我在设置气压传感器采样率寄存器设置时,发现有两个不同的设置,一个是采样次数,一个是过采样,不知道这二者有什么区别?分别需要设置成什么数值?
谢谢!
Hello,
when using this sensor, the communication between the microcomputer and the sensor cannot be realized, can you provide a solution?
Thank you,
Zhang
Show Less