Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Pressure Sensors Forum Discussions

Sort by:
Kenta
Pressure Sensors
I am working on the pressure sensor (DPS310) for my study. The time resolution of the sensor is around 4Hz which I would like to develop. Do you guys ... Show More
ThongTran
Pressure Sensors
Structure of messages transmit (SP40T (SP400-15-11)) to receive (CMT 2219B)? How to read sensor values in SP40T(SP400-15-11) microcontroller? (temper... Show More
ThongTran
Pressure Sensors
Structure of messages transmit (SP40T (SP400-15-11)) to receive (CMT 2219B)? How to read sensor values in SP40T(SP400-15-11) microcontroller? (temper... Show More
Hemn_87
Pressure Sensors
Hi Dears.I want to read parameter from sensor by sending command through out I2C for the SP370 (900 kPs) In programming Mode.I can read Temp and Volta... Show More
cant66
Pressure Sensors
Dear  infineon, do you have or do you have in roadmap a similar barometric absolute Pressure sensor with high accuracy like the ST LPS22HH ? Thanks a ... Show More
Forum Information

Pressure Sensors

Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.