Pressure Sensors Forum Discussions
I'm using SP49 TPMS sensor example code.
My query is: How can I stop the interval timer in this code?
As there is no such library function for this. I couldn't find a way to stop the interval timer.
Show LessI'm using example code of SP49 sensor.
How can I add .c and .h files to the existing code and compile them?
Hi,
I've noticed the DPS310 pressure sensor now has "not for new design" label in the product finder. Can you please recommend alternatives in similar price range?
Also, are there any information regarding the DPS310 status available? For how long it will be produced, supported etc.? I've tried to find it but without any success.
Thanks and have a nice day!
Best regards,
Michal Šebesta
Based on the device acceleration (acceleration sensor value) how to wake up the device? In example code where we can set the Acceleration sensor threshold value for wakeup.
Show Lessin the driver sensor-xensiv-dps3xx-master.zip (downloaded from https://github.com/Infineon/sensor-xensiv-dps3xx), there are two files with license texts (LICENSE & EULA).
Which of the two license text is the current one? Where can I request this information?
Thank you very much
Thomas
芯片: KP229E2701 ,C1 、C2我们贴的都是100nf ;但实际测试出来C1: 130nf, C2:230nf; C2的值为什么差的那么大?
Dear Team
We are starting a project on which we are willing to measure ambient pressure by means of single KP264 chip.
Our project run in the ISO26262 context and we are wondering if such device can support ISO 26262, so we are interested to maximum SPF\LPF and PHMHF this sensor can reach from pressure measurement function perspective .
Infineon classify this as Class II compoenent and s "ISO 26262 Ready" Classo it should support the integrator with sort of safety analysis or light form of safety manual (called SAN) to help the evaluation of above metrics
Is this SAN content supporting FMEDA with any FIT estimation and failure mode partition both at PIN and internal Functional level ?
Is this documentation available already in the web site or is it distributed under NDA ?
Thanks
VIMA1974
Show Less
Hello,
We are aware that C4115 most likely indicates a special PN, but need to know if there are any differences in fit, form or function to the standard PN or not?
If there is a datasheet you can share - that would also be perfect. If not, just the differences would be enough.
Background - we have received this PN: KP235C4115XTMA1 from Infineon and need to understand if customers can use it or not.
Thanks,
Katie
Show LessI bought SP4X_DEV_KIT, how can I get an example code?
Please tell me how I can download the example code
And,,Question about "SP400-15-11" (TPMS Pressure Sensor).
If the pressure measurement range of the sensor is 100 to 1,400 kPa, and the actual pressure exceeds 1400 kPa, how does the sensor recognize it?
I wonder if the sensor cannot measure or if it recognizes and informs you of the maximum measurement range of 1,400kPa
When the actual pressure exceeds 1,400kPa, I would like to know what the SP400-15-11 element tells me.
(ex, When the actual pressure is 1,500 kPa, is the value that the sensor tells me 1,400 kPa?)
Show LessWhat is the difference between KP235 and KP235C4115? We received KP235C4115 on a recent purchase and noticed the output was 300mv higher than the KP235 and the absolute pressure reported was higher than the true pressure.
Show Less