Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Forum Discussions

Browse the Community

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.

1128143 901

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.

611171 423

HEMT (GaN)

Infineon’s CoolGaN™ is a highly efficient GaN (gallium nitride) transistor technology for power conversion in the voltage range up to 600V. The pioneering quality ensures the highest standards and offers the most reliable and performing solution among all GaN HEMTs on the market. Switched-mode power circuits using CoolGaN™ can benefit from the improved energy efficiency and the improved power density, which is not possible with state-of-the-art silicon devices. In this forum, you can post your questions, comments, and feedback about CoolGaN™ devices and their applications.

69198 39

Diodes & Thyristors (Si/SiC)

Infineon being a market leader for power diodes and thyristors, offers core technology for wide range of application ranging from power level of 10kW to 10GW. We offer high efficient silicon or CoolSiC™ silicon carbide diodes in discrete housings as well as bare dies for the highest flexibility, with both industrial and automotive qualification. In this forum, you can post your questions, comments and feedback about any diode/ thyristor part from Infineon. You can even sign up for our free Newsletter to receive first-hand news and update.

103265 79

Smart Power Switches

The Smart Low-Side & High-Side Switches forum is designed for you to post your questions, comments and feedback about all our market’s most comprehensive portfolio of smart power switches like PROFET™, HITFET™, SPOC™, SPIDER and FLEX product families. Ask your technical questions or explore existing content!

278973 211

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.

1803055 419

LED Driver ICs

Infineon provides innovative, high-performance LED Driver ICs solutions that incorporate best-in-class technologies and can be used in a wide range of LED lighting applications including Automotive and Industrial Lighting. In this forum, you can post your questions, comments, and feedback about the LED driver products and evaluation boards offered by Infineon. You can even sign up for our free Newsletter to receive first-hand news and update.

234035 146

Intelligent Power Modules (IPM)

Post your questions about Infineon Intelligent Power Modules (IPMs). Depending on the level of integration and power required there are different options of semiconductors and drivers in numerous packages for various voltage and current classes. CIPOS™ IPMs are families of highly integrated, compact power modules designed to drive motors in applications ranging from home appliances to fans, pumps, and general-purpose drives

212258 68

Class D Audio Amplifier IC

In this forum you can post your questions, comments and feedback about the Infineon Merus range of mid power and high power Class D Amplifiers that range from 10Watts to 5kW! Infineon’s Merus Audio amplifiers range from Analog Input Discrete Class D amplifiers for Home, Professional and Aftermarket Automotive amplifiers through to highly integrated digital I2S input Class D amplifiers for portable and home active speakers. Post your questions below to get feedback from our team of audio experts. For the quickest response please share parts of your schematic, layout and configuration data. Below you’ll also find links to the latest board pages, GitHub, documents and FAQs.

200319 98

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.

1659250 705

Power Management ICs

Discussion forum related to Power Management topics covering the following product groups: <br><br> <li>OPTIREG™ PMIC</li> <li>OPTIREG™ SBCs</li> <li>OPTIREG™ Linear</li> <li>OPTIREG™ Switcher</li> <li>DC-DC Converters</li> <li>AC-DC Power Conversion</li> <li>Automotive Conventional Powertrain ICs</li> <li>Wireless Charging ICs</li> <li>Isolated Industrial Interface</li> <li>Contactless power and sensing ICs</li> <li>Solid State Relay</li> <br> Ask your technical questions or explore existing content!

1407463 704

Contactless power and sensing ICs

Welcome to the NFC Tag Side Controller NAC1080 and NGC1081 Forum! Explore and discuss the capabilities of these microcontrollers, including energy harvesting, NFC communication, and motor control. Connect with developers, share experiences, and learn about integrating these controllers into projects like IoT, smart devices, and industrial automation. Join now to unlock (pun intended) new possibilities!

15730 29
filter icon

Featured Discussions

Sort by:
YuTa_4942221
MOSFET (Si/SiC)
Thank you always.Let me confirm one point regarding 1200V discrete SiC. 【question】Is it possible to receive FBSOA for IMZA120R030M1H and IMZA120R040M1... Show More
Clyasenth
Smart Power Switches
Hi, I am using TLE9104SH as a low-side switch. I want to control it with IN1,2,3,4, not from SPI. According to the datasheet, for enabling the output ... Show More
PaulojM
Motor Control ICs
Hi, I am trying to use a USB to UART converter, connecting it to TX/RX 0 and program the imc102T with the MCEDesigner. Normally, i can do it without a... Show More
Translation_Bot
Gate Driver ICs
This is about the gate driver of 2ED2181S06F. This is an existing product with a built-in bootstrap diode, but does it also have a limiting resistor b... Show More
Raj08
Gate Driver ICs
Hello,  I am trying to study the 1k6W PSU Link .I am unable to understand the connections of Oring MOSFET gate driver (secondary side), specifically  ... Show More
Zhouzy
MOSFET (Si/SiC)
i am reading the datasheet of TLE9183.and there is some description about crc3 in page 22 : The CRC generator polynomial is x^3+x^1+1.The seed value i... Show More
Jhon01
IGBT
While in the midst of integrating the Speakatoo API into my project, I've encountered an error pertaining to cookies. I'm reaching out to seek assista... Show More
Translation_Bot
Diodes & Thyristors (Si/SiC)
  Hello Does Infineon have any solution for IEC-1000-4-6 (not IEC 1000-4-5)) who applies RF (150K~8M)stress which is current injection ? Customer says... Show More
Translation_Bot
Power Management ICs
I am trying to program IRPS5401 via i2c. I believe I followed the Rocky programming guide, apart from the VOUT register, effectively changed its confi... Show More
Translation_Bot
Power Management ICs
Hello friend Is there a code example for TLF30682QVS01? I use Aurix dev studio with Ava board [24V Car Gateway]. In MyICP, the code provided in the fo... Show More