Power Management ICs Forum Discussions
I know it is possible to power it with a DC supply but can a standard USB adaptor (only with only 5V output be used if only asking for 5W charging? I have tried changing many of the settings in the wireless configuration tool - removing the non 5V PDOs, setting the max current to 1.5A etc but charging will not start using a standard wall adapter (non PD).
If not the reference board can the WLC1115 be setup to use 5V wall adapters? As we are doing a custom design based on the reference board.
Show LessI am trying to program IRPS5401 via i2c. I believe I followed the Rocky programming guide, apart from the VOUT register, effectively changed its configuration CAN... I attached a screenshot of the difference between the registers and the registers in memory in the file. I program everything through i2c as stated in the manual, but am I missing any steps to allow VOUT changes?
Thank you very much.
Show LessHello friend
Is there a code example for TLF30682QVS01? I use Aurix dev studio with Ava board [24V Car Gateway]. In MyICP, the code provided in the folder [ADS_AG_24V_LWIP_HTTPD_V1.0.1] does not contain the source for this toggle PS. If WD is included that needs to be serviced, otherwise the MCU is reset.
For other products, such as TLE94, there is a configuration wizard that allows you to generate code. But TLF30682QVS01 is not good?
Thank you
Show LessHi all,
We would like to have QTP report of MB570PF-G-BND-K5ERE1/MB571PF-G-BND-K5ERE1.
We understood those are EOLed devices.
Customer just need this data for internal registration.
Please check and give us some advice.
BR,
Uehara
Show LessI'm here to talk about two circuit component inventions of mine, the Biode and Transratiometer. These inventions are silicon or semiconductor based logical processing elements, which are capable of reducing computer circuit complexity to 1/2 the original number of parts. In addition, computers may become up to 2x as fast and efficient by implementing these technologies. Check out the circuit diagrammes I've rewritten and talked about in my scientific paper.
These devices can be made the same way as diodes and transistors, for the biode and transratiometer respectively, as p/n, n/p/n junctions. Many people ask me how they are produced, but I promise you they are produced equivalently to diodes and transistors - just with a different number of outputs.
I have produced halfway functional models by modifying transistors and diodes, but I do not have the laboratory to produce real models. I come here today to look for research partners or sponsorship.
Here's the paper:
https://www.dropbox.com/s/cntd1fn27jc7zeb/BIODES%20AND%20TRANSRATIOMETERS.pdf?dl=0
P.S. A lot of my circuit diagrammes use resistors in the schematics, but as modern computers do not use resistors so often anymore, but rather have diodes doing the work of the resistor, they can be substituted with diodes in my schematics and the reduction of parts and function remains the same.
E-mail me at bagels105oranges@gmail.com if interested.
Show LessPower Management ICs
Ask your technical questions or explore existing content!