Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Management ICs Forum Discussions

Sort by:
Brice
Power Management ICs
Hello IFX partner, For TLE7259-3GE, "Suitable for 12 V and 24 V board net" It is currently used in 24V systems, the maximum supply voltage will up to ... Show More
Skykraft
Power Management ICs
I am working with development kits TLE9015DQU AND AURIX TFT boards. Going through the manual, it states:Select the *.hex file “Infineon_TLE9015DQU_TLE... Show More
Luc
Power Management ICs
How to prevent some copycats read the patch bin file data which has been stored to OTP in the XDPP1100 controller via I2C or other communication inter... Show More
ATYQ
Power Management ICs
Hello Community, Can you help me please. I use QSPI to communicate between TC36x and TLE9471-3ES I can't understand the difference between Status Info... Show More
cirkit
Power Management ICs
i have designed and developed a 24V 3A CV power supply board on ICL8810. The design requirements are 1) input 100-300V AC 2) output 24V 3A 3) PF > 0.9... Show More
wgq
Power Management ICs
当上电进入INIT模式在 INIT timer 到期之前发生了导致进入INIT模式的故障,图片所示,比如ERR pin故障,会发生 INIT -> INIT 吗?   还是说只有timer到期才会发生? Show More
Dennis
Power Management ICs
    According to the IEC TR 62380 formula provided below, might I get your assist to obtain the value of  λ based on the parameters λ1 and λ2 from t... Show More
tonycstech
Power Management ICs
OpenPower, i am unable to flash XDPE132G5DBoth dongle and chip were purchased form mouser.I am able to flash IR35217 using same dongle with PowerCenen... Show More
iCatlett
Power Management ICs
Hello, I am using the REFWLCTX15WC1 reference design with the source code given from Modus Toolbox and I am trying to limit my output transmitter powe... Show More
geminikowui
Power Management ICs
now I need design the request as follow: input: 12V-dc output current: 10~100A /constant current   output volotage: 2~9V can you introduct the design ... Show More
Forum Information

Power Management ICs

Discussion forum related to Power Management topics covering the following product groups:

  • OPTIREG™ PMIC
  • OPTIREG™ SBCs
  • OPTIREG™ Linear
  • OPTIREG™ Switcher
  • DC-DC Converters
  • AC-DC Power Conversion
  • Automotive Conventional Powertrain ICs
  • Wireless Charging ICs
  • Isolated Industrial Interface
  • Contactless power and sensing ICs
  • Solid State Relay

  • Ask your technical questions or explore existing content!