Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Management ICs Forum Discussions

MS_19060803
Power Management ICs
いつもお世話になっております。 概略回路図と波形を添付いたします。 デバイスが起動する60V時のシャント抵抗RCS波形を測定していると、波形⑥で デバイスの電流リミット(0.8V)以上の波形(約1.19V)が測定されました。 データシートを確認する限り0.8Vは超える事はないと考えているのですが、 ... Show More
Korbinian
Power Management ICs
Hi, I am planning to use the SS1 output of the TLF35584. I don't fully understand how the output behaves when the SBC is in the safe state. Is the out... Show More
IzzetKorkmaz
Power Management ICs
Hi, I am trying to set sbc to sleep mode but i guess due to the current value sbc switch wake state directly. To be ensure i try to read the wake up r... Show More
ashok1987
Power Management ICs
Hi, I tried to get the information about the peak current rating of ICE3PCS01G internal drivers but I think this info is not avilable in datasheet... ... Show More
wph1995
Power Management ICs
Hello, We are designing the controller of a peltier cell, I want to control the peltier cell using an h-bridge made with N-MOSFET, so I would like to ... Show More
sbl
Power Management ICs
Hi,I have a WLC1115 evaluation board and while testing it I encountered this problem. It can't charge our receiver (in this case the led satatus of ev... Show More
drudolf
Power Management ICs
I submitted a question previously on the Power Solutions:  https://www.infineon.com/cms/en/product/promopages/Altera/Arria10StratixX100Wto160W/ It was... Show More
mona
Power Management ICs
i have a IR38164MTRPBFAUMA1 ic mounted on a board with a NXP processor (T2080) with a ferritebead which was kept open initially.The IR38164MTRPBFAUMA1... Show More
IzzetKorkmaz
Power Management ICs
Hi, I try to set the sleep mode via TLF35585 but the board consuming a almost 160 mA which is higher than settable monitoring current value (max value... Show More
drormo7
Power Management ICs
Hello, I do redesign to pfc board with your component: IR1155STRPBF that become obsolite. I chose in ICE2PCS01GXUMA1 as alternative part ,and I have a... Show More
Forum Information

Power Management ICs

Discussion forum related to Power Management topics covering the following product groups:

  • OPTIREG™ PMIC
  • OPTIREG™ SBCs
  • OPTIREG™ Linear
  • OPTIREG™ Switcher
  • DC-DC Converters
  • AC-DC Power Conversion
  • Automotive Conventional Powertrain ICs
  • Wireless Charging ICs
  • Isolated Industrial Interface
  • Solid State Relay

  • Ask your technical questions or explore existing content!