Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Power Management ICs Forum Discussions

Sort by:
matus
Power Management ICs
Hello, I was wondering where I could find the design files for the above mentioned Xilinx boards?  I can't find them at https://www.infineon.com/cms/en/product/promopages/xilinx-SoC-FPGA-power-reference-design/Xilinx_Zynq_UltraScale_RFSoC/... Show More
Marcelo_Macedo1
Power Management ICs
Hi, Can you please help providing the step-by-step to enable the output voltage for IR38263 using PMBus? I'm trying to help a customer but as we don't... Show More
yogeshks1
Power Management ICs
Hi  we are looking a simple cost effective buck converter Input DC Is +55VDC output DC is 35VDC, load current at 35VDC is 3A. can you suggest a cost e... Show More
Ottabe1
Power Management ICs
I have a need to use Wireless Power to charge the batteries in some equipment used for asset tracking. I don't care about having a trademarked logo on... Show More
sbl
Power Management ICs
Hi,In our project, we want to communicate the WLC1115 with a microcontroller  via UART but there are no pins available.  - The SCB1 is configured as U... Show More
iCatlett
Power Management ICs
Hello, I am currently working with the REF WLCTX15WC evaluation board, and I am using the example source code from Modus Toolbox. I found the macro, C... Show More
GerVel94
Power Management ICs
I have 2 configurations for TLD7002-16 ES in ocfg file. one of them has values in GPIN0 (used to tail light function) and the second doesnt have value... Show More
臭猫
Power Management ICs
tle9461 intn
solved msg Solved
tle9461的intn引脚的内部弱下拉何时会被触发,目前客户原理图有外部上拉47k下拉0k,是否会对产品有影响.
Robert1
Power Management ICs
I am currently using ICE3PCS01G to design a circuit, the specifications are as follows: VIN_AC=85V~265V; Vout=312V; 300W; VCC=15V. At present, the tes... Show More
Nachiket_Wawoo
Power Management ICs
TLF35584
solved msg Solved
Hello Experts,As per attached image, the problem which i am facing is that the QUC 3V3 signal is not rising till 3.3V and also TLF is going in FAILSA... Show More
Forum Information

Power Management ICs

Discussion forum related to Power Management topics covering the following product groups:

  • OPTIREG™ PMIC
  • OPTIREG™ SBCs
  • OPTIREG™ Linear
  • OPTIREG™ Switcher
  • DC-DC Converters
  • AC-DC Power Conversion
  • Automotive Conventional Powertrain ICs
  • Wireless Charging ICs
  • Isolated Industrial Interface
  • Contactless power and sensing ICs
  • Solid State Relay

  • Ask your technical questions or explore existing content!