Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Power Management ICs Forum Discussions

Sort by:
geminikowui
Power Management ICs
now I need design the request as follow: input: 12V-dc output current: 10~100A /constant current   output volotage: 2~9V can you introduct the design ... Show More
Andyli
Power Management ICs

ICE3PCS01G,PFC电路,高温50℃老化,中途,VB_OK信号消失,是怎么回事?

Luc
Power Management ICs
How to prevent some copycats read the patch bin file data which has been stored to OTP in the XDPP1100 controller via I2C or other communication inter... Show More
Luc
Power Management ICs
What's the difference between STORE_DEFAULT_ALL and STORE_USER_ALL, and what's the difference between "Default Store memory" and "User Store memory" i... Show More
Wilson_Sun
Power Management ICs
Hi Team,    烦请教下,这个92464无电流时,开路和对地能报么?谢谢!     Show More
tonycstech
Power Management ICs
OpenPower, i am unable to flash XDPE132G5DBoth dongle and chip were purchased form mouser.I am able to flash IR35217 using same dongle with PowerCenen... Show More
iCatlett
Power Management ICs
Hello, I am using the REFWLCTX15WC1 reference design with the source code given from Modus Toolbox and I am trying to limit my output transmitter powe... Show More
cirkit
Power Management ICs
i have designed and developed a 24V 3A CV power supply board on ICL8810. The design requirements are 1) input 100-300V AC 2) output 24V 3A 3) PF > 0.9... Show More
Sakthivel
Power Management ICs
Hello There,   We are designing a new product for automotive applications (like ECUs) that is powered by an input source of 9 to 36 V, and the ambient... Show More
jpottaway
Power Management ICs
Hi, We are doing a design based on WLC1115 and are using the reference board as a starting point. We have noted that the board does not appear to be c... Show More
Forum Information

Power Management ICs

Discussion forum related to Power Management topics covering the following product groups:

  • OPTIREG™ PMIC
  • OPTIREG™ SBCs
  • OPTIREG™ Linear
  • OPTIREG™ Switcher
  • DC-DC Converters
  • AC-DC Power Conversion
  • Automotive Conventional Powertrain ICs
  • Wireless Charging ICs
  • Isolated Industrial Interface
  • Contactless power and sensing ICs
  • Solid State Relay

  • Ask your technical questions or explore existing content!