XDPP1100

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Sudheer
Level 1
Level 1
First like received First question asked Welcome!

Hey,

Good Day!

 

Can PCB Cu traces be used as a current sense resistor in XDPP 1100 controller? If yes, then how to calculate trace resistance and what layout guidelines needs to be followed?

 

Thank you!

1 Solution
lock attach
Attachments are accessible only for community members.
SuhasBobade
Moderator
Moderator
Moderator
100 sign-ins 50 replies posted 25 solutions authored

Hi VinayKumar,

 

Thanks for posting.

 

The high resolution of IADC allows the XDPP1100 sense output current through very small PCB copper shunt,

saving power loss and cost of precision sense resistor and Op-Amp. Use the following equation to calculate

copper trace resistance.

 

𝑅𝑐𝑜𝑝𝑝𝑒𝑟 = 𝜌 ∙(𝐿/(𝑇 ∙ 𝑊))∙ (1 + 𝑡𝑐 ∙ (𝑡𝑒𝑚𝑝 − 25))

 

ρ: resistivity of copper, 17 ∙ 10−6 𝛺 𝑚𝑚

L: Length of the copper trace

W: Width of the copper trace

T: Thickness of the copper trace

tc: temperature coefficient, 3.9 ∙ 10−3 /˚C

temp: trace temperature, unit ˚C

 

The thickness of copper trace is usually rated in ounces and represents the thickness of 1 ounce of copper

rolled out to an area of 1 square of foot. 1 oz. copper has a thickness of 1.4 mils or 0.0356 mm. Here is a design

example of copper shunt: 130 mil x 100 mil (L x W), top layer, 4 Oz copper, trace resistance is 0.158 mΩ.

 

It is recommended to layout the copper trace shunt in the first mid layer, so that the XDPP1100 controller could

be placed right on top of the shunt trace for the shortest routing distance. Also put a ground shielding layer

next to the copper sense layer to reduce stray inductance for better current sense accuracy. please refer attached image.

 

Kindly let me know if you need any other information.

Thanking you.

View solution in original post

0 Likes
1 Reply
lock attach
Attachments are accessible only for community members.
SuhasBobade
Moderator
Moderator
Moderator
100 sign-ins 50 replies posted 25 solutions authored

Hi VinayKumar,

 

Thanks for posting.

 

The high resolution of IADC allows the XDPP1100 sense output current through very small PCB copper shunt,

saving power loss and cost of precision sense resistor and Op-Amp. Use the following equation to calculate

copper trace resistance.

 

𝑅𝑐𝑜𝑝𝑝𝑒𝑟 = 𝜌 ∙(𝐿/(𝑇 ∙ 𝑊))∙ (1 + 𝑡𝑐 ∙ (𝑡𝑒𝑚𝑝 − 25))

 

ρ: resistivity of copper, 17 ∙ 10−6 𝛺 𝑚𝑚

L: Length of the copper trace

W: Width of the copper trace

T: Thickness of the copper trace

tc: temperature coefficient, 3.9 ∙ 10−3 /˚C

temp: trace temperature, unit ˚C

 

The thickness of copper trace is usually rated in ounces and represents the thickness of 1 ounce of copper

rolled out to an area of 1 square of foot. 1 oz. copper has a thickness of 1.4 mils or 0.0356 mm. Here is a design

example of copper shunt: 130 mil x 100 mil (L x W), top layer, 4 Oz copper, trace resistance is 0.158 mΩ.

 

It is recommended to layout the copper trace shunt in the first mid layer, so that the XDPP1100 controller could

be placed right on top of the shunt trace for the shortest routing distance. Also put a ground shielding layer

next to the copper sense layer to reduce stray inductance for better current sense accuracy. please refer attached image.

 

Kindly let me know if you need any other information.

Thanking you.

0 Likes