XDPP1100

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
navsuh
Level 1
Level 1
First reply posted First question asked Welcome!

Can XDPP1100 digital power controller can be used for building 6000W-200A or 9000W-300A power supplies.

0 Likes
1 Solution
Sodum
Moderator
Moderator
Moderator
50 solutions authored 250 sign-ins 10 likes given

Hello @navsuh ,

XDPP1100 is typically designed for medium voltage DC-DC applications.

With this IC, Vin is limited to 127V, Iout maximum to 127A per phase, and 255A maximum Iout with interleaved PSFB.

To support higher input voltage or higher output current, a Firmware patch is required to scale the resolution and range.

Please refer to the below link for the reference design of an evaluation board (which uses this Firmware patch), designed to support Vin till 400V.

https://www.infineon.com/cms/en/product/evaluation-boards/vd_1000w_gan_psfb_xdp/

Regards,

Premsagar S 

View solution in original post

0 Likes
3 Replies
Sodum
Moderator
Moderator
Moderator
50 solutions authored 250 sign-ins 10 likes given

Hello @navsuh ,

Thank you for posting your query on Infineon Community.

Can you please provide the following details of your design,

  • Voltage ratings of Input & Output.
  • Current ratings of Input & Output.
  • Application.
  • Selected power stage topology & switching frequency. 

Regards,

Premsagar S

0 Likes
navsuh
Level 1
Level 1
First reply posted First question asked Welcome!

Hello Premsagar S ,

  • Voltage ratings of Input & Output are 540V DC, 30V-50V DC.
  • Current ratings of Input & Output  20A-30A, 200A-300A.
  • Application-welding and cutting.
  • Selected power stage topology & switching frequency are Full bridge or half bridge,100KHZ-200KHZ,current mode/PCMC. 
Thank You
Naveed
0 Likes
Sodum
Moderator
Moderator
Moderator
50 solutions authored 250 sign-ins 10 likes given

Hello @navsuh ,

XDPP1100 is typically designed for medium voltage DC-DC applications.

With this IC, Vin is limited to 127V, Iout maximum to 127A per phase, and 255A maximum Iout with interleaved PSFB.

To support higher input voltage or higher output current, a Firmware patch is required to scale the resolution and range.

Please refer to the below link for the reference design of an evaluation board (which uses this Firmware patch), designed to support Vin till 400V.

https://www.infineon.com/cms/en/product/evaluation-boards/vd_1000w_gan_psfb_xdp/

Regards,

Premsagar S 

0 Likes