Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Mithun
Level 1
Level 1
First like given 5 sign-ins First reply posted

Product: TLE4296-2G V50

Looking for current thresholds for the Current Limit and the Short Circuit limit. (Overload Protection).

Also looking for the temperature thresholds for thermal shutdown and recovery. (Overtemperature Protection)

 

Would be nice if someone could provide this information.

0 Likes
1 Solution
AnilKumar
Moderator
Moderator
Moderator
First question asked 50 solutions authored 10 likes received

Hello,

Infineon’s automotive linear regulators are designed to withstand junction temperatures up to 150°C.

To prevent IC damage in fault conditions (e.g. output continuously short-circuited), a thermal shutdown has been integrated. The circuitry switches off the power stage for a junction temperature higher than 151°C, typically 175°C, unless otherwise specified in the datasheet. The device re-starts automatically after cooling down with a typical hysteresis of 15K (e.g. with a thermal shut-down at 175°C, re-start occurs at 160°C). 

Please refer to the below document under the chapter "Embedded Protection"->Thermal Shutdown.

https://www.infineon.com/dgdl/Introduction%20to%20Automotive%20Linear%20Voltage%20Regulators%20BR-20...

Thanks

Anil

View solution in original post

3 Replies
Vishnu_Nambrath
Moderator
Moderator
Moderator
50 solutions authored 100 replies posted 5 likes given

Hello, 

Overload protection starts with 30mA output load current. 
Hence it is safe to operate in applications where the load current is lower than 30mA. 

The safe operating junction temperature is up to 150C. I am checking internally for the thermal shutdown limit. 
I shall come back to you once I have this information. 

Regards 
Vishnu N

 

0 Likes

Thanks for the quick response. Looking forward.

0 Likes
AnilKumar
Moderator
Moderator
Moderator
First question asked 50 solutions authored 10 likes received

Hello,

Infineon’s automotive linear regulators are designed to withstand junction temperatures up to 150°C.

To prevent IC damage in fault conditions (e.g. output continuously short-circuited), a thermal shutdown has been integrated. The circuitry switches off the power stage for a junction temperature higher than 151°C, typically 175°C, unless otherwise specified in the datasheet. The device re-starts automatically after cooling down with a typical hysteresis of 15K (e.g. with a thermal shut-down at 175°C, re-start occurs at 160°C). 

Please refer to the below document under the chapter "Embedded Protection"->Thermal Shutdown.

https://www.infineon.com/dgdl/Introduction%20to%20Automotive%20Linear%20Voltage%20Regulators%20BR-20...

Thanks

Anil