Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Power Management ICs Forum Discussions

chpa_4701971
Level 1
Level 1

my application runs on 2.5 A peak current when data packet transmitting. I want to use solar charger IC S6AE102A/S6AE103A.

In datasheet Maximum output current (Normal mode) IOUTLD1 shows minimum value 10mA, but there is no Max Iout value shown. can anyone comment, what maximum load I can run on this IC ?

0 Likes
1 Solution
EijiF_46
Employee
Employee
10 likes received First like received

It is difficult to support 2.5A peak current using S6AE102A and 103A.

Internal VOUT resistor of S6AE102A/ 103A is max: 2.5-OHM. In case of VOUT:3.3V, the maximum current will be 1.32 A.

Thanks

Fukawa

View solution in original post

0 Likes
1 Reply
EijiF_46
Employee
Employee
10 likes received First like received

It is difficult to support 2.5A peak current using S6AE102A and 103A.

Internal VOUT resistor of S6AE102A/ 103A is max: 2.5-OHM. In case of VOUT:3.3V, the maximum current will be 1.32 A.

Thanks

Fukawa

0 Likes