- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
my application runs on 2.5 A peak current when data packet transmitting. I want to use solar charger IC S6AE102A/S6AE103A.
In datasheet Maximum output current (Normal mode) IOUTLD1 shows minimum value 10mA, but there is no Max Iout value shown. can anyone comment, what maximum load I can run on this IC ?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It is difficult to support 2.5A peak current using S6AE102A and 103A.
Internal VOUT resistor of S6AE102A/ 103A is max: 2.5-OHM. In case of VOUT:3.3V, the maximum current will be 1.32 A.
Thanks
Fukawa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It is difficult to support 2.5A peak current using S6AE102A and 103A.
Internal VOUT resistor of S6AE102A/ 103A is max: 2.5-OHM. In case of VOUT:3.3V, the maximum current will be 1.32 A.
Thanks
Fukawa