- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am using IR3564B PMIC in our custom design board. In the datasheet(February 24, 2015 | V1.1) we received with NDA, the recommended operating temperature given as "0/+85 (page 😎 " but in some parts of the datasheet, it is given as -40 +85 (page 1). Which information is correct and what is the operation junction temperature of the IC.
Another issue;
Could you suggest other PMIC with AMD SVI2 interface?
Thanks.
Solved! Go to Solution.
- Labels:
-
ispn:10345:1:0
-
l1:144:1:0
-
l2:199:1:0
-
l3:280:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Emre_Kahraman ,
IR3564B can operate from -40°C to 85°C ambient temperature, but the recommended operating temperature (system accuracy & other key parameters are guaranteed) is 0°C to 85°C. If the ambient temperature is beyond the recommended temperature range derating should be considered. Please refer to note 3 in the datasheet for these details. IR3564B is a NRND part.
You can consider XDPE14283A, this part supports AMD SVI2 interface.
Regards,
Premsagar S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Emre_Kahraman ,
IR3564B can operate from -40°C to 85°C ambient temperature, but the recommended operating temperature (system accuracy & other key parameters are guaranteed) is 0°C to 85°C. If the ambient temperature is beyond the recommended temperature range derating should be considered. Please refer to note 3 in the datasheet for these details. IR3564B is a NRND part.
You can consider XDPE14283A, this part supports AMD SVI2 interface.
Regards,
Premsagar S