ICE3PCS01G,PFC电路,高温50℃老化,中途,VB_OK信号消失

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Andyli
Level 1
Level 1
First question asked First reply posted Welcome!

ICE3PCS01G,PFC电路,高温50℃老化,中途,VB_OK信号消失,是怎么回事?

0 Likes
1 Solution
Neo_Qin
Moderator
Moderator
Moderator
5 likes given 250 replies posted 250 sign-ins

Hi @Andyli ,

在整个Tj工作温度范围内(-25 °C to 125 °C), 根据芯片手册中的表4.39,虽然VB_OK引脚的Source电流来自VREF(6mA max),但其本身只有1mA 的负载能力。当Tamb= 50°C时,IC的结温有可能已经接近上限,此时VB_OK实际上已经很难维持高于规格值的带载能力。

Neo_Qin_0-1695377743846.png

因此,如果直接使用VB_OK直接驱动光耦的输入是有风险的,我仍然建议您参考我们的典型设计,仅将VB_OK作为控制信号使用,驱动三极管或MOS管进行功率放大后再驱动光耦,源一般选择VCC。

BR,

Neo

View solution in original post

0 Likes
6 Replies
Neo_Qin
Moderator
Moderator
Moderator
5 likes given 250 replies posted 250 sign-ins

Hi @Andyli ,

感谢您对英飞凌产品的使用。

VB_OK信号与母线电压,以及VBTHL_EN的阈值设置有关。

您可以提供异常发生时的VCC/VREF/VBTHL_EN/VSENSE波形吗?

在测试时,您有监控IC的壳温吗?

另外,您可以分享您的原理图吗,我想确认参数设置是否有问题。

 

期待您的反馈。

BR,

Neo

0 Likes
Andyli
Level 1
Level 1
First question asked First reply posted Welcome!

您好,VB_OK消失这种现象具有偶发性,但一台发生基本上这台必发生,只抓取了VB_OK信号发生异常时的VB_OK分压电压和PFC输出的电压情况,如图。

如果您方便,电话沟通较为方便和快捷,希望得到你们的指导。我的电话是:15063632003

0 Likes
Neo_Qin
Moderator
Moderator
Moderator
5 likes given 250 replies posted 250 sign-ins

Hi @Andyli ,

在整个Tj工作温度范围内(-25 °C to 125 °C), 根据芯片手册中的表4.39,虽然VB_OK引脚的Source电流来自VREF(6mA max),但其本身只有1mA 的负载能力。当Tamb= 50°C时,IC的结温有可能已经接近上限,此时VB_OK实际上已经很难维持高于规格值的带载能力。

Neo_Qin_0-1695377743846.png

因此,如果直接使用VB_OK直接驱动光耦的输入是有风险的,我仍然建议您参考我们的典型设计,仅将VB_OK作为控制信号使用,驱动三极管或MOS管进行功率放大后再驱动光耦,源一般选择VCC。

BR,

Neo

0 Likes
Andyli
Level 1
Level 1
First question asked First reply posted Welcome!

Hi Neo_Qin,

谢谢您的解答。

VB_OK规格书要求的最大输出电流的最小保证值是1mA,我们设计时应保证最大输出电流不应大于1mA,这个信息有用,谢谢。

还有个问题,VB_OK既然有电流限制,我们测试到VB_OK超过一定的电流后VB_OK信号会丢失,不应该是维持恒流状态吗?难道VB_OK输出做了过流保护?有这部分的功能图做支撑吗?规格书上没有提及

 

0 Likes
Neo_Qin
Moderator
Moderator
Moderator
5 likes given 250 replies posted 250 sign-ins

Hi @Andyli ,

作为普通的应用工程师,我们也没有更详细的IC内部框图。

根据我个人的理解,Reference Voltage Block只能作为一个普通的电压源使用,其内部电路中并没有输出电流反馈回路(一个间接的证据是外围电路中并没有专门针对VREF电流的采样),因此Reference Voltage Block无法在恒压源和恒流源的角色之间进行切换。

这也意味着当VB_OK输出电流超出规格值后,VREF(含VB_OK)既无法维持当前电流的恒定输出,也不能保证输出电压满足后级光耦输入发光二极管的正向压降需求。

Neo_Qin_0-1695606427192.png

IC的规格中一般包含一定的冗余,当结温较低时,VB_OK超规格驱动光耦有一定的成功概率,但其驱动能力一定随着结温的升高而下降。由于您的光耦只是用来传递对后级DCDC的使能控制信号,如果对传输延时没有特殊要求,可以尝试将发光二极管的限流电阻设置在5k以上,或更换CTR值更大的光耦看目前的现象是否有所改善。

BR,

Neo

0 Likes
Andyli
Level 1
Level 1
First question asked First reply posted Welcome!

Hi Neo_Qin,

我们先实验用VB_OK单独推动NPN去驱动光耦,高温老化,看看还会不会出现这个问题,有结果再进行反馈,谢谢。

0 Likes