Can the overvoltage protection of S6AE101A work normally when the input is high voltage and low current?

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
XiLi_4790246
Level 1
Level 1

Given in the data sheet:

"When the VDD pin voltage exceeds the OVP detection voltage (VOVPH = 5.4V), an OVP protection current (IOVP) flows from the VDD pin to suppress the rise of the VDD pin voltage and prevent damage to the IC. In addition, when it drops below the OVP release voltage (VOVPL = 5.3V), the flow of OVP protection current is stopped. "

And the electrical characteristics table gives:

"OVP protection current(Iovp)minimum value is 6mA."

If the power source has high impedance and the output is high voltage (hundred volts) and low current (microamps),  can the OVP module of S6AE101A work normally and stably for a long time under this condition?

Is there a voltage/current limit range of the input for the OVP part?

0 Likes
1 Solution
EijiF_46
Employee
Employee
10 likes received First like received

Hi

Yes. The OVP of S6AE101A can work normally and stably for a long time under this condition.

There is no voltage limit range.

The current limit range is up to 6mA. When you'd like to use high-current power source (6mA or more), the external OVP circuit on PCB is required.

Thanks

View solution in original post

2 Replies
EijiF_46
Employee
Employee
10 likes received First like received

Hi

Yes. The OVP of S6AE101A can work normally and stably for a long time under this condition.

There is no voltage limit range.

The current limit range is up to 6mA. When you'd like to use high-current power source (6mA or more), the external OVP circuit on PCB is required.

Thanks