windows 8 driver

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   

Win8 does not seem to recognize miniprog3 driver.  Is there a win8 driver it??

   

TJ

0 Likes
8 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

I do not think Win 8 driver released yet, see

   

 

   

http://www.cypress.com/?app=forum&id=2233&rID=70652

   

 

   

and recent - http://www.cypress.com/?rID=56745

   

 

   

Try posting a tech case at www.cypress.com and ask for the schedule of Win 8 driver

   

release.

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Thanks Dana. 

   

I opened a case, will post their response.

   

 

   

TJ

0 Likes
lock attach
Attachments are accessible only for community members.
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

Would you like to have a try with below workaround:

   
    1)            Copy the "drivers" folder under C:\Program Files (x86)\Cypress\Programmer\3.xx\ directory of a Win7 machine which has the PSoC Programmer software being installed (or download the attached "drivers.zip" file, in case you don't have a Win7 machine which has PSoC Programmer installed).   
   
    2)            Put it in your Win8 machine under "C:\Program Files (x86)\Cypress\Programmer\3.xx" directory(unzip the "drivers.zip" file as a folder if you use the attached).   
   
    3)            Run the "driver.bat" file in the "drivers" folder on Win8 machine.   
   
    4)            Now any kit(MiniProg kit included) who used PSoC Programmer should be working with Win8 64bit machine.   
   

Regards,

   

Roy

Roy Liu
0 Likes
Anonymous
Not applicable

 Thank you Roy.  That did the trick and miniprog3 gets connected.

   

Happy New Year, all the best to PSoCers!

   

TJ

0 Likes
JoHo_299991
Level 1
Level 1

 I am having the exact same issue but the above steps didn't help me. Very disappointing really.

0 Likes
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

 Hello Jose,

   

Can you provide more info about the failure with your Win8 machine?

   

There is another thread talking about this,  http://www.cypress.com/?app=forum&id=2232&rID=74548

   

and seems the workaround is same. I have been received multiple success feedback, so, Would you please give it more try?

   

Regards.

   

Roy

Roy Liu
0 Likes
Anonymous
Not applicable

thanks, worked like a charm 🙂

0 Likes
Anonymous
Not applicable

Problem with MinIprog3 and Programmer drivers is resolved with Programmer 3.19.1.

   

If you have Windows 8.1, then same problem may occur in this as well. Solution for this problem is available at link http://www.cypress.com/?app=forum&id=2492&rID=89646. In a tech support case, Cypress support person told me that they are going to fix the problem of drivers with Windows 8.1 in upcoming version of PSoC Programmer.

   

 

   

-Rave

0 Likes