Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

Anonymous
Not applicable

 Hi all,

   

I added a new custom component to my project.

   

this component is built from several different blocks  (with integration between them).

   

also, I added some API files (C source code + C header). but, when I try to build this component the API files are not compiled.

   

how can I make the build operation compile the API files with all the other component elements? 

   

thanks.

0 Likes
1 Reply
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

This works usually without any special commands. I presume you have red the "Components Author Guide" which was installed into your Cypress directory already. You did not specify whether you are working with PSoC1 in opposite to 3,4 and 5.

   

When you post your complete project, we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file (do NOT use chrome, that still may not work).

   

 

   

Bob
 

0 Likes