- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I would like to create an embedded mySQL client running on PSoC (PSoC 6, to be specific). I will connect to the Internet via a Ublox SARA module.
I've found a few Open Source mySQL connectors for Arduino, and these could be adapted, but I wonder if anyone has already done this for PSoC, or general 'C', especially if they've already done the glue to the UBLOX AT command set.
Thanks!
Larry
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Larry,
I'm afraid no has one has ported any mysql connectors from Arduino Libraries to PSoC. But there is an open source library available in C which can be used: MySQL :: MySQL 8.0 Reference Manual :: 28.7.1 MySQL C API Implementations
But we haven't done anything of this nature, so cannot guarantee its working. If your application requirement is to connect to a mySQL database, then I would suggest using the PSoC 6 WiFi-BT to connect to the internet and use AWS to host the database. We have some AWS code examples which you can refer: Cypress Semiconductor | Mbed
Regards,
Dheeraj