Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

Anonymous
Not applicable

How or where do I find 'kit packages' to install for Creator?

   

ie, for the CY8CKIT-049-42xx 

   

When I run Creator (3.0), under the Examples and Kit bar, it shows "No kit pacakges installed"

0 Likes
11 Replies
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Here at bottom of page -

   

 

   

    

   

          http://www.cypress.com/?rID=92146

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

I see that...and have dowmloaded it to my machine..

   

How does that get installed as a 'kit package' in the Creator tool?

   

(Parhaps this was the wrong kit to use an an example, as I see it references use a 'example project downloaded')

   

Are there other kits that will appear in the Creator tool?

   

From the tool itself:

   

Kits

   

This link provides a hierarchical list of the installed kits, along with their associated sample projects. You can obtain kits from the Cypress web site.

   
        
  • The top level shows the name of the kits. Click on one of them to view the documentation for that kit.
  •     
  • Under each kit, you will see sample projects. Click on one of them to create a copy of the example and open it in PSoC Creator. You will be asked where to save the project.
  •    
   

Note If you install any kits while PSoC Creator is running, click the Refresh icon to view those kits. The list will expand to show you what kits are installed.

0 Likes
HeLi_263931
Level 8
Level 8
100 likes received 50 likes received 25 likes received

There are no kit files for the -049 kit. When you look at e.g. the -050 kit page, you find the DVK files packaged in an installer. Executing this one will make the files appear in Creator.

0 Likes
Anonymous
Not applicable

https://youtu.be/v-ZHFygeL2I?t=3m27s indicates what a -049 kit should look like.

   

I executed the files at as you direct above (I THINK???)  

   

named CY8CKIT050BSetupOnlyPackage.exe

   

But the -049 kit shown in the video still does not appear for me in the PSoC Creator 3.3

   

Could you help direct me to which files I am missing?  

   

Maybe it would help if you linked a specific file, or gave the exact filename of the DVK file I should be using on the -050 kit page.

   

Thank you,

   

-AJ

0 Likes
Anonymous
Not applicable

And, I have found it.  

   

AT https://youtu.be/v-ZHFygeL2I?t=3m11s into this video, I was baffled about exactly WHAT file to download and install to see the displayed installed kit. I searched for hours, because this section of the video is very ambiguous.

   

The download file that I needed is actually this one:

   

http://www.cypress.com/file/184941/download

   

And, it's on this page:

   

http://www.cypress.com/documentation/development-kitsboards/psoc-4-cy8ckit-049-4xxx-prototyping-kits

   

And, it's called

   

CY8CKIT-049-42xx Kit Only (Kit Design Files, Documentation, Examples) 

   

CY8CKIT04942xxSetupOnlyPackage_revSA.exe

   

I hope this helps others.

   

I also documented this as a comment in the YouTube video that I reference above.

   

Best everyone,
-AJ

   

 

   

 

   

 

   

 

   
        

To shorten your next search:

   

Enter "CY8CKIT-049-42xx" into the Keywords field at top of this page. 2 clicks later you can download and install the examples.

   

I would suggest you to get hands on a CY8CKIT-043 Prototyping kit. As a beginner it is very much easier having debugging capabilities for just a few bucks more. You still can use your -049 board to execute a well tested and debugged project.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thanks for the excellent tip, very helpful, I had sucess at the first try! (Install CY8CKIT04942xxSetupOnlyPackage_revSA.exe)

0 Likes
Anonymous
Not applicable

makes more sense now... thanks for the explanation.

0 Likes
HeLi_263931
Level 8
Level 8
100 likes received 50 likes received 25 likes received

When installing the -050 kit files, you can have a look at twhere the files go. It might be possible to put the -049 example projects in a similar location to make them appear in Creator...

0 Likes
markgsaunders
Employee
Employee
50 sign-ins 10 solutions authored 5 solutions authored

Yes, the 049 kits are a little simpler than the usual kits we ship. Instead of installing into the Start Page you just grab the projects from the web page.

   

Do you guys have a preference?

   

I like the speed of getting projects directly, but I also like the installed kits because I have just one place to go look and a quick way to create a new project.

   

-- Mark.

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

The installed versions are handled by Cypress update manager, so

   

have a maintenance/change advantage.

   

 

   

Regards, Dana.

0 Likes