- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
how to assign the values for the buttons and the sliders, while using the PSoC--CY8C20534 for e.g. void display_update_LEDs(BYTE sensor_state) { LED_0_Switch( (sensor_state & 0x02) ); LED_1_Switch( (sensor_state & 0x04) ); LED_2_Switch( (sensor_state & 0x08) );
}
please explain me the coding below---- //Set port drive modes for LEDs
PRT0DM0 |= 0b00100010; //strong on P0[5],P0[1]
PRT0DM1 &=~0b00100010;
PRT1DM0 |= 0b10100100; //strong on P1[2]
PRT1DM1 &=~0b10100100;
PRT2DM0 |= 0b10100000; //strong on P2[5],P2[7]
PRT2DM1 &=~0b10100000;
Regards--
Amit
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The PRTxDM0 & PRTxDM1 register sets the drive mode of a pin in
a specific port.
The code is to set and clear bits in the two registers to set the
drive mode of a specific pin in a specific port.
It looks like PRT0 and PRT2 are done right, but PRT1 comments
one pin is being set when in fact it is touching 3 pins.
Look at the register TRM for definitions for these registers. I show
DM0, you should also look at DM1.
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
thanks Dana, I got the use of the two regi. DM0 & DM1. right now I'm using it as the follow- void display_update_LEDs(BYTE sensor_state) { LED_0_Switch( (sensor_state & 0x02) ); LED_1_Switch( (sensor_state & 0x04) ); LED_2_Switch( (sensor_state & 0x08) ); LED_2_Switch( (sensor_state & 0x10) ); LED_2_Switch( (sensor_state & 0x01) );
} in this I'm getting the buttons sesing right, but what I haven't got is placing of those values
for e.g. 0x02, 0x04, 0x08, 0x10 etc, how to assign the values for the buttons and the sliders, while using the PSoC--CY8C20534
-----
Amit
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Those values correspond to the pin in a port.
So -
0x01 Pin 0
0x02 Pin 1
0x04 Pin 2
0x08 Pin 3
0x10 Pin 4
0x20 Pin 5
0x40 Pin 6
0x80 Pin 7
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Dana, I tried your suggestios but the are not working. I think its something about the raw count.
can you explain me this RAW COUNT thing.
I'm using the instruction
WORD sensor_raw_count;
is it the same or else, please explain.
----
Amit
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content