Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

Anonymous
Not applicable

I downloaded your PSOC 5 object library for Segger's emWin Graphics library.  However, the only driver I see is the GUIDRV_CompactColor_16.c.  I am using the Sitronix ST7529 LCD controller.  Does Cypress happen to have this LCD driver?  If not, do I need to go to Segger direct?

   

Thanks.

   

jsonder

0 Likes
2 Replies
crcac_264396
Level 4
Level 4
First like received

I've been poking around with this myself (http://www.cypress.com/?app=forum&id=2492&rID=58742).

   

From what I understand, and some one please correct me, is there are two drivers provided by Cypress. One runs on the controller-less graphics peripheral, and the other is the GUIDRV_CompactColor_16 driver. Both are configured to run in a parallel bus setup.

   

According to Segger documentation, the GUIDRV_CompactColor_16 runs the following display controllers:

   

 

   

Himax HX8301, HX8312A, HX8347

   

Hitachi HD66766, HD66772, HD66789

   

Ilitek ILI9161, ILI9220, ILI9320, ILI9325

   

LG Electronics LGDP4531

   

MagnaChip D54E4PA7551

   

Novatek NT39122, NT7573

   

OriseTech SPFD5408, SPFD5420A

   

Renesas R63401, R61509, R61516, R61505

   

Samsung S6D0110A, S6D0117, S6D0129

   

Sharp LR38825, LCY-A06003

   

Sitronix ST7712, ST7628, ST7637

   

Solomon SSD1289

   

Toshiba JBT6K71

   

Epson S1D13743

   

 

   

 

   

I understand that from Segger you can acquire other drivers. Maybe get a copy of GUIDRV_Template from them and you/we can customize? They most likely have already written exactly what you need though.

0 Likes
crcac_264396
Level 4
Level 4
First like received

 Oh, since you have a sitronix with similar product number, maybe the compact color driver can be altered with some defines -- I noticed somewhere in the code there were defines that indicated register locations and commands. Of course I forget the exact spot

0 Likes