Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ Creator & Designer Forum Discussions

ChVa_3548136
Level 2
Level 2
Welcome!

I'm having a problem with PSoC Creator crashing repeatedly.  I have version 4.2 installed, and the latest crash was when it was loading the workspace.

The crashes don't seem to limited to any one workspace (I have a few) or activity, although I have a programmer plugged in most of the time.

I'm running Windows 10 Home 1803 64 bit.

Here is the info from Windows Event Viewer:

Faulting application name: psoc_creator.exe, version: 0.0.0.0, time stamp: 0x5a85e2fd

Faulting module name: ucrtbase.dll, version: 10.0.17134.165, time stamp: 0x9de2441b

Exception code: 0xc0000409

Fault offset: 0x000a27ab

Faulting process id: 0x338

Faulting application start time: 0x01d425a61e84006e

Faulting application path: C:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\bin\psoc_creator.exe

Faulting module path: C:\WINDOWS\System32\ucrtbase.dll

Report Id: 4a4582ff-2e8c-4e6c-9deb-d54138f8cf1d

Faulting package full name:

Faulting package-relative application ID:

Thanks for any help,

Chris VanBrederode

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Looks like a problem with your display driver. I'm running the same windows version as you do and I have no problems at all.

Bob

View solution in original post

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Looks like a problem with your display driver. I'm running the same windows version as you do and I have no problems at all.

Bob

0 Likes

I've updated the display drivers, and it's only happened once since then.

0 Likes